![Logo](ti_logo.svg) |
AM62Px MCU+ SDK
09.01.00
|
|
Go to the documentation of this file.
40 #ifndef SDL_SOC_DCC_H_
41 #define SDL_SOC_DCC_H_
47 #include <sdl/include/am62px/sdlr_soc_baseaddress.h>
61 #define SDL_DCC_MAX_INSTANCE (11U)
118 SDL_DCC5_BASE, SDL_DCC6_BASE, SDL_DCC7_BASE, SDL_DCC8_BASE, \
119 SDL_MCU_DCC0_BASE, SDL_MCU_DCC1_BASE};
static uint32_t SDL_DCC_baseAddress[SDL_DCC_MAX_INSTANCE]
Definition: sdl_soc_dcc.h:117
@ SDL_DCC_INST_MCU_DCC0
Definition: sdl_soc_dcc.h:88
@ SDL_DCC_INST_DCC7
Definition: sdl_soc_dcc.h:83
@ SDL_DCC_INST_DCC4
Definition: sdl_soc_dcc.h:77
@ SDL_DCC_INST_DCC0
Definition: sdl_soc_dcc.h:69
SDL_DCC_Inst
Enum for different DCC module instances supported.
Definition: sdl_soc_dcc.h:67
@ SDL_DCC_INST_DCC8
Definition: sdl_soc_dcc.h:85
@ SDL_DCC_INST_DCC3
Definition: sdl_soc_dcc.h:75
@ SDL_DCC_INVALID_INSTANCE
Definition: sdl_soc_dcc.h:93
@ SDL_DCC_INST_DCC5
Definition: sdl_soc_dcc.h:79
@ SDL_DCC_INST_DCC1
Definition: sdl_soc_dcc.h:71
int32_t SDL_DCC_getBaseaddr(SDL_DCC_Inst instance, uint32_t *baseAddr)
This API is used to get the base address of the instance.
#define SDL_DCC_MAX_INSTANCE
MAX number of supported DCC Instances.
Definition: sdl_soc_dcc.h:61
@ SDL_DCC_INST_DCC2
Definition: sdl_soc_dcc.h:73
@ SDL_DCC_INST_MCU_DCC1
Definition: sdl_soc_dcc.h:90
@ SDL_DCC_INST_DCC6
Definition: sdl_soc_dcc.h:81