This example demonstrates how to configure the DCC and use it to monitor clocks in the two supported modes (continuous and single-shot modes). It also demonstrates how to receive errors generated by DCC in the MCU and Main domain.
This example displays:
* Initializing the ESM to detect the DCC error event(s) * Registration of application callback for notification of ESM error events for the MCU ESM instance * Configuration of one MCU DCC instance to monitor a single clock in continuous mode * Forcing of an error to create a DCC error event
The following methods can be used as a trigger for the DCC error event:
* Change ratio criterion for stable clocks * Use Sciclient API to change clock dividers (with ratio criterion stable) to speed up clock * Use Sciclient API to change clock dividers (with ratio criterion stable) to slow down clock * Turn off power for the monitored input clock
Use Case | Reference Clock | Description |
---|---|---|
UC-1 | HFOSC0 | Configuration of MCU DCC instance in continuous mode and error event is forced |
UC-2 | HFOSC0 | Configuration of MCU DCC instance in single-shot mode and completion with no errors |
UC-3 | HFOSC0 | Configuration of MCU DCC instance in continuous mode and completion with no errors |
UC-4 | RC OSC | Configuration of MCU DCC instance in single-shot mode and completion with no errors |
UC-5 | RC OSC | Configuration of DCC instance in continuous mode and error event is forced |
UC-6 | RC OSC | Configuration of DCC instance in continuous mode and error event is forced |
UC-7 | HFOSC0 | Configuration of DCC instance in continuous mode and error event is forced |
UC-8 | RC OSC | Configuration of DCC instance in continuous mode and completion with no errors |
Parameter | Value |
---|---|
CPU + OS | mcu-r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am62px-sk |
Example folder | examples/sdl/dcc/dcc_app/ |
Shown below is a sample output when the application is run,