Introduction
This example demonstrates setting of multiple LED at the same time connected to the same I2C controller. The application will blink all the I2C controlled LED in the EVM.
Application exits after 10 iterations..
Supported Combinations
Parameter | Value |
CPU + OS | mcu-r5fss0-0 nortos |
wkup-r5fss0-0 freertos |
Toolchain | ti-arm-clang |
Boards | am62px-sk |
Example folder | examples/drivers/i2c/i2c_led_blink |
AM62X-SK
- Watch out for LED LD2 to blink which is controlled by I2C1.
Steps to Run the Example
- Attention
- As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.
See Also
I2C
Sample Output
Shown below is a sample output when the application is run,
I2C LED Blink Test Started ...
LED will Blink for 10 loop ...
I2C LED Blink Test Passed!!
All tests have passed!!