AM62L FreeRTOS SDK  11.02.00
Driver Porting Layer (DPL) demo

Introduction

This example shows a simple application, which setups the CPU and the underlying RTOS or no-RTOS environment on the supported SOC.

The example does the below

  • Setup a timer with system tick of 1ms, setup MPU and cache (if available)
  • Create a RTOS task (in RTOS example)
  • Trigger a ISR and signal a semaphore from ISR to main task
  • Show usage of clock delay
  • Show usage of cache APIs
  • Show usage of heap APIs

Supported Combinations

Parameter Value
CPU + OS a53ss0-0 nortos
a53ss0-0 freertos
a53ss0-1 nortos
a53ss0-1 freertos
Toolchain arm.gnu.aarch64-none
Board am62lx-evm
Example folder examples/kernel/dpl/dpl_demo/

Steps to Run the Example

See Also

Driver Porting Layer (DPL)

Sample Output

Shown below is a sample output when the application is run,

[DPL] Hwi post ...
[DPL] Hwi post ... DONE !!!
[DPL] Sleep for 100 msecs ...
[DPL] Sleep ... DONE (Measured time = 100000 usecs, CPU cycles = 80000055 ) !!!
[DPL] Running cache operations ...
[DPL] Running cache operations ... DONE !!!
[DPL] Heap free size = 1984 bytes
[DPL] Allocated 1023 bytes @ 0x80010440, heap free size = 896 bytes
[DPL] Free'ed 1023 bytes @ 0x80010440, heap free size = 1984 bytes
All tests have passed!

FreeRTOS-AMP Sample Output

Shown below is a sample output on UART0 console (logs for a53ss0-0) when the application is run,

DPL Demo Example started on a53_core0
[DPL] Hwi post ...
[DPL] Hwi post ... DONE !!!
[DPL] Hwi(sgi) post ...
[DPL] Hwi(sgi) post ... DONE !!!
[DPL] Sleep for 100 msecs ...
[DPL] Sleep ... DONE (Measured time = 99052 usecs, CPU cycles = 107978 ) !!!
Note: In case of FREERTOS CPU Cycles will not match with the measured time
As the "WFI" instruction is called from idle task, which suspends the PMU counter used to measure CPU cycles.
[DPL] Running cache operations ...
[DPL] Running cache operations ... DONE !!!
[DPL] Heap free size = 1984 bytes
[DPL] Allocated 1023 bytes @ 0x82020440, heap free size = 896 bytes
[DPL] Free'ed 1023 bytes @ 0x82020440, heap free size = 1984 bytes
All tests have passed on a53_core0 !!

Shown below is a sample output on UART1 console (logs for a53ss0-1) when the application is run,

DPL Demo Example started on a53_core1
[DPL] Hwi post ...
[DPL] Hwi post ... DONE !!!
[DPL] Hwi(sgi) post ...
[DPL] Hwi(sgi) post ... DONE !!!
[DPL] Sleep for 100 msecs ...
[DPL] Sleep ... DONE (Measured time = 99181 usecs, CPU cycles = 107091 ) !!!
Note: In case of FREERTOS CPU Cycles will not match with the measured time
As the "WFI" instruction is called from idle task, which suspends the PMU counter used to measure CPU cycles.
[DPL] Running cache operations ...
[DPL] Running cache operations ... DONE !!!
[DPL] Heap free size = 1984 bytes
[DPL] Allocated 1023 bytes @ 0x88020440, heap free size = 896 bytes
[DPL] Free'ed 1023 bytes @ 0x88020440, heap free size = 1984 bytes
All tests have passed on a53_core1 !!