AM62L FreeRTOS SDK  11.02.00
Empty Project

Introduction

This is an empty project provided for all cores present in the device. User can use this project to start their application by adding more SysConfig modules.

This application does driver and board init and just prints the pass string on the console. In case of the main core, the print is redirected to the UART console. For all other cores, CCS prints are used.

Supported Combinations

Parameter Value
CPU + OS a53ss0-0 nortos
a53ss0-0 freertos
a53ss0-1 nortos
a53ss0-1 freertos
Toolchain arm.gnu.aarch64-none
Board am62lx-evm
Example folder examples/empty/

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

All tests have passed!!

FreeRTOS-AMP Sample Output

Shown below is a sample output on UART0 console (logs for a53ss0-0) when the application is run,

All tests have passed on a53_core0 !!

Shown below is a sample output on UART1 console (logs for a53ss0-1) when the application is run,

All tests have passed on a53_core1 !!