AM62L FreeRTOS SDK  11.02.00
MCASP Playback

Introduction

This example demostrates the McASP configured for an audio playback mode of operation. A headset with mic needs to be connected to the auido jack on am62lx-evm. The audio from the microphone will be played back to both the headset (Left & Right).

  • Mcasp is configured in I2S mode
  • Data transfer is on both channels (Left and Right)

Supported Combinations

Parameter Value
CPU + OS a53ss0-0 freertos
Toolchain arm.gnu.aarch64-none
Board am62lx-evm
Example folder examples/drivers/mcasp/mcasp_playback_codec_aic32

Steps to Run the Example

See Also

MCASP

Sample Output

Shown below is a sample output when the application is run,

[MCASP] Audio playback example started.
Enter your response on UART terminal
Stop the demo? (y/n) : y