|
AM62D FreeRTOS SDK
12.00.00
|
|
Go to the documentation of this file.
73 #include <drivers/hw_include/soc_config.h>
75 #if defined (DRV_VERSION_UDMA_V0)
78 #include <drivers/udma/v0/include/csl_udmap_cppi5.h>
79 #include <drivers/udma/v0/include/csl_pktdma_cppi5.h>
80 #if (UDMA_NUM_UTC_INSTANCE > 0)
81 #include <drivers/hw_include/cslr_dru.h>
90 #include <drivers/udma/v0/hw_include/csl_bcdma.h>
91 #include <drivers/udma/v0/hw_include/csl_intaggr.h>
92 #include <drivers/udma/v0/hw_include/csl_lcdma_ringacc.h>
93 #include <drivers/udma/v0/hw_include/csl_pktdma.h>
97 #if defined (DRV_VERSION_UDMA_V1)
98 #include <drivers/udma/v1/soc/udma_soc.h>
99 #include <drivers/udma/v1/include/udma_types.h>
100 #include <drivers/udma/v1/include/udma_ring.h>
101 #include <drivers/udma/v1/include/udma_flow.h>
102 #include <drivers/udma/v1/include/udma_event.h>
103 #include <drivers/udma/v1/include/udma_rm.h>
104 #include <drivers/udma/v1/include/udma_ch.h>
105 #include <drivers/udma/v1/include/csl_udmap_tr.h>
106 #include <drivers/udma/v1/include/csl_udmap_cppi5.h>
107 #include <drivers/udma/v1/include/csl_pktdma_cppi5.h>
108 #include <drivers/udma/v1/include/udma_utils.h>
109 #include <drivers/udma/v1/hw_include/csl_bcdma.h>
110 #include <drivers/udma/v1/hw_include/csl_lcdma_ringacc.h>
111 #include <drivers/udma/v1/hw_include/csl_pktdma.h>
149 typedef void *(*Udma_PhyToVirtFxn)(uint64_t phyAddr,
317 typedef struct Udma_DrvObject_t
uint32_t instId
Definition: udma.h:164
UDMA Low Level Driver SOC specific file.
int32_t Udma_deinit(Udma_DrvHandle drvHandle)
UDMA deinit function.
UDMA ring related parameters and API.
UDMA utility API to make TR, get TR descriptor memory requirement.
UDMA initialization parameters.
Definition: udma.h:163
UDMA RM related parameters and API.
uint8_t enableUtc
Definition: udma.h:168
UDMA resource manager init parameters.
Definition: udma_rm.h:172
Udma_PhyToVirtFxn phyToVirtFxn
Definition: udma.h:181
Udma_VirtToPhyFxn virtToPhyFxn
Definition: udma.h:176
UDMA event related parameters and API.
UDMA Low Level Driver API/interface data types file.
uint64_t Udma_defaultVirtToPhyFxn(const void *virtAddr, uint32_t chNum, void *appData)
Default virtual to physical translation function.
uint64_t(* Udma_VirtToPhyFxn)(const void *virtAddr, uint32_t chNum, void *appData)
UDMA Virtual to Physical address translation callback function.
Definition: udma.h:134
This file provides support for the UDMAP Transfer Request (TR) functionality.
Udma_RmInitPrms rmInitPrms
Definition: udma.h:166
int32_t Udma_init(Udma_DrvHandle drvHandle, const Udma_InitPrms *initPrms)
UDMA init function.
void * Udma_DrvHandle
UDMA driver handle.
Definition: udma_types.h:65
void *(* Udma_PhyToVirtFxn)(uint64_t phyAddr, uint32_t chNum, void *appData)
UDMA Physical to Virtual address translation callback function.
Definition: udma.h:149
UDMA Channel related parameters and API.
int32_t UdmaInitPrms_init(uint32_t instId, Udma_InitPrms *initPrms)
Udma_InitPrms structure init function.
Opaque UDMA driver object.
Definition: udma.h:318
UDMA flow related parameters and API.
void * Udma_defaultPhyToVirtFxn(uint64_t phyAddr, uint32_t chNum, void *appData)
Default physical to virtual translation function.
uint32_t skipGlobalEventReg
Definition: udma.h:170