AM62D FreeRTOS SDK  12.00.00
bootloader_soc.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2021-2023 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef BOOTLOADER_SOC_AM62X_H_
34 #define BOOTLOADER_SOC_AM62X_H_
35 
36 #include <drivers/hw_include/cslr_soc.h>
37 #include <drivers/udma.h>
38 
39 #include <drivers/sciclient/include/tisci/am62x/tisci_hosts.h>
40 
41 /* Self reset config */
42 
43 extern int32_t sproxy_send_msg_r5_to_tifs_fw(void *msg, size_t len);
44 
46 #define WKUP_R5_HOST_ID TISCI_HOST_ID_MAIN_0_R5_1
47 #define SELF_RESET_BOOT_ADDRESS_LOW CSL_WKUP_R5FSS0_CORE0_BTCM_BASE
48 
49 #define FREERTOS_SMP_RPRC_CORE_ID (100U)
50 #define FREERTOS_SMP_NO_OF_CORES (4U)
51 #define FREERTOS_SMP_BOOT_CORE (CSL_CORE_ID_A53SS0_0)
52 #define FREERTOS_SMP_CSL_CORE_ID_MAX (FREERTOS_SMP_NO_OF_CORES + CSL_CORE_ID_A53SS0_0)
53 
54 /* DMA channel type configured by bootloader layer */
55 #define BOOTLOADER_DMA_CHANNEL_TYPE UDMA_CH_TYPE_TR_BLK_COPY
56 
64 typedef struct
65 {
66  uint32_t tisciProcId;
67  uint32_t tisciDevId;
68  uint32_t tisciClockId;
69  uint32_t defaultClockHz;
70  char coreName[8];
71 
73 
82 typedef void __attribute__((__noreturn__)) (*Bootloader_SelfCoreJump)(void);
83 
93 int32_t Bootloader_socCpuRequest(uint32_t cpuId);
94 
104 int32_t Bootloader_socCpuRelease(uint32_t cpuId);
105 
116 int32_t Bootloader_socCpuSetClock(uint32_t cpuId, uint32_t cpuHz);
117 
127 uint64_t Bootloader_socCpuGetClock(uint32_t cpuId);
128 
139 uint32_t Bootloader_socCpuGetClkDefault(uint32_t cpuId);
140 
152 int32_t Bootloader_socCpuPowerOnReset(uint32_t cpuId, void *socCoreOpMode);
153 
165 int32_t Bootloader_socCpuResetRelease(uint32_t cpuId, uintptr_t entryPoint);
166 
172 
177 void __attribute__((__noreturn__)) Bootloader_socSelfCPUjump();
178 
190 int32_t Bootloader_socCpuSetEntryPoint(uint32_t cpuId, uintptr_t entryPoint);
191 
203 uint32_t Bootloader_socTranslateSectionAddr(uint32_t cslCoreId, uint32_t addr);
204 
212 uint32_t Bootloader_socRprcToCslCoreId(uint32_t rprcCoreId);
213 
221 bool Bootloader_socIsSmpEnable(uint32_t rprcCoreId);
222 
229 
237 char* Bootloader_socGetCoreName(uint32_t cpuId);
238 
246 int32_t Bootloader_socMemInitCpu(uint32_t cpuId);
247 
255 uint32_t Bootloader_socGetSciclientCpuProcId(uint32_t cpuId);
256 
264 uint32_t Bootloader_socGetSciclientCpuDevId(uint32_t cpuId);
265 
272 
279 
286 
294 int32_t Bootloader_socAuthImage(uint32_t certLoadAddr);
295 
303 
304 
313 
320 
327 void Bootloader_socCpuPowerOff(uint32_t cpuId);
328 #endif /* BOOTLOADER_SOC_AM64X_H_ */
Bootloader_socCpuSetClock
int32_t Bootloader_socCpuSetClock(uint32_t cpuId, uint32_t cpuHz)
Set the clock of a particular CPU in the AM62x SOC.
Bootloader_socGetCoreName
char * Bootloader_socGetCoreName(uint32_t cpuId)
Get the name of a core.
Bootloader_CoreBootInfo::tisciDevId
uint32_t tisciDevId
Definition: bootloader_soc.h:67
Bootloader_socCpuRequest
int32_t Bootloader_socCpuRequest(uint32_t cpuId)
Request for a particular CPU in the AM62x SOC.
Bootloader_socIsSmpEnable
bool Bootloader_socIsSmpEnable(uint32_t rprcCoreId)
Check whether the smp is enabled or not for the soc.
Bootloader_socCpuPowerOff
void Bootloader_socCpuPowerOff(uint32_t cpuId)
Power off a core.
Bootloader_socIsMCUResetIsoEnabled
uint32_t Bootloader_socIsMCUResetIsoEnabled()
Check if MCU M4 is reset isolated.
Bootloader_socGetSciclientCpuProcId
uint32_t Bootloader_socGetSciclientCpuProcId(uint32_t cpuId)
Obtain the Sciclient Proc Id corresponding to the CSL core ID.
Bootloader_socWaitForFWBoot
int32_t Bootloader_socWaitForFWBoot(void)
API to wait for boot notification from SYSFW/ROM.
Bootloader_socCpuSetEntryPoint
int32_t Bootloader_socCpuSetEntryPoint(uint32_t cpuId, uintptr_t entryPoint)
Set entry point for self CPU in the AM62x SOC from reset.
Bootloader_socIsAuthRequired
uint32_t Bootloader_socIsAuthRequired(void)
API to check if authentication is required for the device. Checks the SYS_STATUS register to see if d...
Bootloader_socCpuPowerOnReset
int32_t Bootloader_socCpuPowerOnReset(uint32_t cpuId, void *socCoreOpMode)
Do power-on-reset of a particular CPU in the AM62x SOC.
Bootloader_CoreBootInfo::defaultClockHz
uint32_t defaultClockHz
Definition: bootloader_soc.h:69
addr
uint64_t addr
Definition: csl_udmap_tr.h:3
Bootloader_socCpuResetRelease
int32_t Bootloader_socCpuResetRelease(uint32_t cpuId, uintptr_t entryPoint)
Release a particular CPU in the AM62x SOC from reset.
sproxy_send_msg_r5_to_tifs_fw
int32_t sproxy_send_msg_r5_to_tifs_fw(void *msg, size_t len)
Bootloader_socGetSciclientCpuDevId
uint32_t Bootloader_socGetSciclientCpuDevId(uint32_t cpuId)
Obtain the Sciclient Device Id corresponding to the CSL core ID.
Bootloader_CoreBootInfo::tisciProcId
uint32_t tisciProcId
Definition: bootloader_soc.h:66
Bootloader_CoreBootInfo
Data structure containing information about a core specific to the AM62x SOC.
Definition: bootloader_soc.h:65
Bootloader_enableMCUPLL
void Bootloader_enableMCUPLL(void)
Enable MCU PLL. The MCU PLL will be initialized by SYSFW if devgrp is set to DEVGRP_ALL....
Bootloader_CoreBootInfo::tisciClockId
uint32_t tisciClockId
Definition: bootloader_soc.h:68
Bootloader_socRprcToCslCoreId
uint32_t Bootloader_socRprcToCslCoreId(uint32_t rprcCoreId)
Obtain the CSL core ID of a CPU from its RPRC core ID.
Bootloader_socCpuGetClock
uint64_t Bootloader_socCpuGetClock(uint32_t cpuId)
Get the clock of a particular CPU in the AM62x SOC.
Bootloader_socCpuRelease
int32_t Bootloader_socCpuRelease(uint32_t cpuId)
Release a particular CPU in the AM62x SOC.
__attribute__
void __attribute__((__noreturn__))(*Bootloader_SelfCoreJump)(void)
Function pointer to jump a self core to specific code location in AM62x SOC.
Definition: bootloader_soc.h:82
udma.h
UDMA Driver API/interface file.
Bootloader_socAuthImage
int32_t Bootloader_socAuthImage(uint32_t certLoadAddr)
API to authenticate (and decrypt if needed) an appimage using SYSFW.
Bootloader_socTranslateSectionAddr
uint32_t Bootloader_socTranslateSectionAddr(uint32_t cslCoreId, uint32_t addr)
Translate a CPU address to the SOC address wherever applicable.
Bootloader_socGetSelfCpuList
uint32_t * Bootloader_socGetSelfCpuList(void)
Get the list of self cpus in the SOC.
Bootloader_socCpuGetClkDefault
uint32_t Bootloader_socCpuGetClkDefault(uint32_t cpuId)
Get the default clock of a particular CPU in the AM62x SOC.
Bootloader_socSecHandover
int32_t Bootloader_socSecHandover(void)
API to trigger the security handover from SYSFW.
Bootloader_socCpuResetReleaseSelf
int32_t Bootloader_socCpuResetReleaseSelf()
Release self CPU in the AM62x SOC from reset.
Bootloader_socOpenFirewalls
int32_t Bootloader_socOpenFirewalls(void)
API to open required firewalls using SYSFW.
Bootloader_socMemInitCpu
int32_t Bootloader_socMemInitCpu(uint32_t cpuId)
Initialize the core memories of a specific core.