AM62D FreeRTOS SDK  12.00.00
CALCRATIO

Introduction

The CalcRatio algorithm is a real-time sample rate ratio estimator designed to track clock mismatch between two asynchronous audio domains. It computes the ratio of output (Tx) to input (Rx) sample counters and applies a Two-stage moving average to deliver a smooth, stable actual ratio for Asynchronous Sample Rate Conversion (ASRC).

Key Features

  • DMA-Counter-Based Ratio Calculation
  • Two-Stage Moving Average
  • One-Shot Noise Rejection
  • High Accuracy Ratio Tracking

Algorithm Overview

The CalcRatio algorithm works as follows:

  1. Initialization (calcRatio_init()) :
    • Initializes the CALC_RATIO module with input and output sample rates.
    • Computes the target ratio (sampleRateOut / sampleRateIn).
    • Resets all internal states:
      • Moving-average buffers
      • Window pointers
      • Accumulated sums
      • Counters and the one-shot flag
    • Prepares the module for accurate ratio estimation.
  2. First Stage Moving Average (MA1) :
    • Applies a 1024-point moving average to the instantaneous ratio.
    • Removes high-frequency noise and sudden spikes.
    • Produces a smoothed ratio that still responds to short-term changes.
  3. Second Stage Filtering (MA2) :
    • Applies a 128-point moving average to the output of MA1.
    • Reduces long-term drift and stabilizes the ratio.
    • Generates a clean, low-noise ratio used by the resampling stage.
  4. Ratio Calculation (calcRatio_exec()) :
    • Reads instantaneous ratio from the TX/RX DMA counters.
    • Uses a one-shot skip to ignore the first noisy measurement.
    • Updates MA1 and MA2 buffers and their accumulated sums.
    • Computes the actual ratio using both filtering stages.
  5. Output (calcRatio_getActualratio())
    • Provides two key ratio values:
      • Target Ratio: Calculated at initialization.
      • Actual Ratio: Filtered, stable ratio for SW_ASRC operation.
    • Thread-safe access using a global semaphore to avoid race conditions.

API Sequence

To use CALC_RATIO, the application should call the following APIs:

API

APIs for CALCRATIO