AM62D FreeRTOS SDK  12.00.00
HW Interrupts

Attention
See also FreeRTOS, NO RTOS for list of CPU specific supported and unsupported features.

Features Supported

  • Register a interrupt callback to a specific CPU number
  • Ability to pass user specific argument to the interrupt callback
  • Enable, disable, restore and clear specific CPU interrupts
  • Enable, disable, restore global CPU interrupt
  • For ARM R5,
    • Ability to specify interrupt as FIQ or IRQ, level or pulse
    • Ability to specify interrupt priority

Features NOT Supported

See also FreeRTOS, NO RTOS for list of unsupported features.

Important Usage Guidelines

  • For ARM R5,
    • TI VIM is the interrupt controller that is supported.
    • HwiP_disable, HwiP_restore, HwiP_enable only affect state of IRQ. FIQ state is not changed
    • Refer ARMv7-R Architecture reference manual and SOC TRM for more details.
  • For ARM A53,
    • GIC V3 is the interrupt controller that is supported.
    • Interrupt numbers 0-15 are for SGI, 16-31 for PPI and 32-255 for SPI.
    • Refer ARMv8-A Architecture reference manual and SOC TRM for more details.
  • On AM62DX,
    CPU type Valid interrupt numbers Valid interrupt priorities
    R5F 0 .. 511 0 (highest) .. 15 (lowest)
    A53 0 .. 255 0 (highest) .. 15 (lowest)
  • On C75,
    • The C75 CPU supports 64 interrupts.
    • The CLEC event ID can be mapped to any of C75 interrupts.
    • If you are configuring software interrupt, then set eventId to HWIP_INVALID_EVENT_ID.
    • While mapping CLEC event ID to interrupt number, refer the below table and avoid overlapping interrupts.
      Module Interrupt number used
      EQEP 5 .. 7
      TIMER 8 .. 15
      I2C 16 .. 20
      GPIO 21
      UART 22 .. 30
      ECAP 25 .. 27
      UDMA 32 .. 48
      EPWM 49 .. 51
      MCASP 53 .. 58
      IPC 59 .. 62
      MCSPI 1, 2, 31, 52, 63
  • On AM62DX,
    CPU type Valid interrupt numbers Valid interrupt priorities
    R5F 0 .. 511 0 (highest) .. 15 (lowest)
  • On C75,
    • The C75 CPU supports 64 interrupts.
    • The CLEC event ID can be mapped to any of C75 interrupts.
    • If you are configuring software interrupt, then set eventId to HWIP_INVALID_EVENT_ID.
    • While mapping CLEC event ID to interrupt number, refer the below table and avoid overlapping interrupts.
      Module Interrupt number used
      TIMER 2 .. 6
      IPC 7 .. 11
      OSPI 13
      MMCSD 14
      I2C 15 .. 19
      MCSPI 20 .. 24
      ECAP 25 .. 30
      UART 22, 32 .. 38
      MCASP 39 .. 48
      EPWM 49 .. 51
      UDMA 52 .. 61
      WDT 62 .. 63
      ASRC 20 .. 29
      Not Used 12, 31

Example Usage

Include the below file to access the APIs,

#include <stdio.h>

Example ISR,

void myISR(void *args)
{
/* my ISR */
}

Example to register a ISR for CPU interrupt 10,

HwiP_Params hwiParams;
HwiP_Object hwiObj;
HwiP_Params_init(&hwiParams);
/* for R5F, interrupt #10 at VIM */
hwiParams.intNum = 10;
/* for M4F, external interrupt #10 at NVIC is
16 internal interrupts + external interrupt number at NVIC
i.e hwiParams.intNum = 16 + 10;
*/
/* for C75, CLEC event ID can be mapped to any of the internal interrupt number
set both event ID and interrupt number
to configure harware clec event #10
hwiParams.eventId = 10;
hwiParams.intNum = 31;
to configure software interrupt #31
hwiParams.eventId = HWIP_INVALID_EVENT_ID;
hwiParams.intNum = 31;
*/
hwiParams.callback = myISR;
hwiParams.args = NULL;
HwiP_construct(&hwiObj, &hwiParams);

Example to disable and restore interrupts across a crtical section

uintptr_t oldIntState;
oldIntState = HwiP_disable();
/* critical section */
HwiP_restore(oldIntState);

API

APIs for HW Interrupts

HwiP_Params
Parameters passed during HwiP_construct.
Definition: HwiP.h:74
HwiP_construct
int32_t HwiP_construct(HwiP_Object *obj, HwiP_Params *params)
Create a Hwi object.
HwiP_Params_init
void HwiP_Params_init(HwiP_Params *params)
Set default values to HwiP_Params.
HwiP.h
HwiP_Params::callback
HwiP_FxnCallback callback
Definition: HwiP.h:77
HwiP_Object
Opaque Hwi object used with the Hwi APIs.
Definition: HwiP.h:93
HwiP_Params::args
void * args
Definition: HwiP.h:78
HwiP_disable
uintptr_t HwiP_disable(void)
Disable all interrupts.
HwiP_restore
void HwiP_restore(uintptr_t oldIntState)
Restores all interrupts to a given state.
HwiP_Params::intNum
uint32_t intNum
Definition: HwiP.h:76