AM62D FreeRTOS SDK  12.00.00
Driver Porting Layer (DPL) demo

Introduction

This example shows a simple application, which setups the CPU and the underlying RTOS or no-RTOS environment on the supported SOC.

The example does the below

  • Setup a timer with system tick of 1ms, setup MPU and cache (if available)
  • Create a RTOS task (in RTOS example)
  • Trigger a ISR and signal a semaphore from ISR to main task
  • Show usage of clock delay
  • Show usage of cache APIs
  • Show usage of heap APIs

Supported Combinations

Parameter Value
CPU + OS a53ss0-0 nortos
a53ss0-0 freertos
a53ss0-1 freertos
a53ss1-0 freertos
a53ss1-1 freertos
a53ss0-0 freertos-smp
c75ss0-0 freertos
mcu-r5fss0-0 nortos
mcu-r5fss0-0 freertos
r5fss0-0 freertos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
Board am62dx-evm
Example folder examples/kernel/dpl/dpl_demo/

Steps to Run the Example

See Also

Driver Porting Layer (DPL)

Sample Output

Shown below is a sample output when the application is run,

[DPL] Hwi post ...
[DPL] Hwi post ... DONE !!!
[DPL] Sleep for 100 msecs ...
[DPL] Sleep ... DONE (Measured time = 100000 usecs, CPU cycles = 80000055 ) !!!
[DPL] Running cache operations ...
[DPL] Running cache operations ... DONE !!!
[DPL] Heap free size = 1984 bytes
[DPL] Allocated 1023 bytes @ 0x80010440, heap free size = 896 bytes
[DPL] Free'ed 1023 bytes @ 0x80010440, heap free size = 1984 bytes
All tests have passed!

FreeRTOS-AMP Sample Output

Attention
Output from a53ss0-1, a53ss1-0 and a53ss1-1 cores are log to the Shared memory, can be viewed via a53ss0-0 on which log reader is enabled

Shown below is a sample output on UART0 console when the application is run,

DPL Demo Example started on a53_core0
[DPL] Hwi post ...
[DPL] Hwi post ... DONE !!!
[DPL] Hwi(sgi) post ...
[DPL] Hwi(sgi) post ... DONE !!!
[DPL] Sleep for 100 msecs ...
[a530-1] 0.001324s : DPL Demo Example started on a53_core1
[DPL] Hwi post ...335s :
[a530-1] 0.001344s : [DPL] Hwi post ... DONE !!!
[a530-1] 0.001350s : [DPL] Hwi(sgi) post ...
[a530-1] 0.001354s : [DPL] Hwi(sgi) post ... DONE !!!
[a530-1] 0.001357s : [DPL] Sleep for 100 msecs ...
[a531-0] 0.003061s : DPL Demo Example started on a53_core2
[DPL] Hwi post ...071s :
[a531-0] 0.003081s : [DPL] Hwi post ... DONE !!!
[a531-0] 0.003086s : [DPL] Hwi(sgi) post ...
[a531-0] 0.003090s : [DPL] Hwi(sgi) post ... DONE !!!
[a531-0] 0.003093s : [DPL] Sleep for 100 msecs ...
[a531-1] 0.003068s : DPL Demo Example started on a53_core3
[DPL] Hwi post ...078s :
[a531-1] 0.003088s : [DPL] Hwi post ... DONE !!!
[a531-1] 0.003093s : [DPL] Hwi(sgi) post ...
[a531-1] 0.003098s : [DPL] Hwi(sgi) post ... DONE !!!
[a531-1] 0.003101s : [DPL] Sleep for 100 msecs ...
[a530-1] 0.101003s : [DPL] Sleep ... DONE (Measured time = 99642 usecs, CPU cycles = 180095 ) !!!
[DPL] Sleep ... DONE (Measured time = 99473 usecs, CPU cycles = 11895359 ) !!!
Note: In case of FREERTOS CPU Cycles will not match with the measured time
As the "WFI" instruction is called from idle task, which suspends the PMU counter used to mea.
[DPL] Running cache operations ...
[DPL] Running cache operations ... DONE !!!
[DPL] Heap free size = 1984 bytes
[DPL] Allocated 1023 bytes @ 0x80020440, heap free size = 896 bytes
[DPL] Free'ed 1023 bytes @ 0x80020440, heap free size = 1984 bytes
All tests have passed on a53_core0 !!
[a530-1] 0.101008s : Note: In case of FREERTOS CPU Cycles will not match with the measured time
[a530-1] 0.101012s : As the "WFI" instruction is called from idle task, which suspends thes
[a530-1] 0.101016s : ure CPU cycles.
[a530-1] 0.101019s : [DPL] Running cache operations ...
[a530-1] 0.101023s : [DPL] Running cache operations ... DONE !!!
[a530-1] 0.101027s : [DPL] Heap free size = 1984 bytes
[a530-1] 0.101032s : [DPL] Allocated 1023 bytes @ 0x86010440, heap free size = 896 bytes
[a530-1] 0.101037s : [DPL] Free'ed 1023 bytes @ 0x86010440, heap free size = 1984 bytes
[a530-1] 0.101042s : All tests have passed on a53_core1 !!
[a531-0] 0.103003s : [DPL] Sleep ... DONE (Measured time = 99906 usecs, CPU cycles = 179601 ) !!!
[a531-0] 0.103008s : Note: In case of FREERTOS CPU Cycles will not match with the measured time
[a531-0] 0.103012s : As the "WFI" instruction is called from idle task, which suspends thes
[a531-0] 0.103016s : ure CPU cycles.
[a531-0] 0.103019s : [DPL] Running cache operations ...
[a531-0] 0.103023s : [DPL] Running cache operations ... DONE !!!
[a531-0] 0.103027s : [DPL] Heap free size = 1984 bytes
[a531-0] 0.103032s : [DPL] Allocated 1023 bytes @ 0x88010440, heap free size = 896 bytes
[a531-0] 0.103038s : [DPL] Free'ed 1023 bytes @ 0x88010440, heap free size = 1984 bytes
[a531-0] 0.103042s : All tests have passed on a53_core2 !!
[a531-1] 0.103003s : [DPL] Sleep ... DONE (Measured time = 99898 usecs, CPU cycles = 180235 ) !!!
[a531-1] 0.103008s : Note: In case of FREERTOS CPU Cycles will not match with the measured time
[a531-1] 0.103012s : As the "WFI" instruction is called from idle task, which suspends thes
[a531-1] 0.103016s : ure CPU cycles.
[a531-1] 0.103019s : [DPL] Running cache operations ...
[a531-1] 0.103023s : [DPL] Running cache operations ... DONE !!!
[a531-1] 0.103027s : [DPL] Heap free size = 1984 bytes
[a531-1] 0.103032s : [DPL] Allocated 1023 bytes @ 0x8a010440, heap free size = 896 bytes
[a531-1] 0.103038s : [DPL] Free'ed 1023 bytes @ 0x8a010440, heap free size = 1984 bytes
[a531-1] 0.103043s : All tests have passed on a53_core3 !!