AM62D FreeRTOS SDK  12.00.00
Hello World Project

Introduction

This example just does driver and board initialization and prints the string, Hello World! on UART console.

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 nortos
mcu-r5fss0-0 freertos
a53ss0-0 nortos
a53ss0-0 freertos
a53ss0-1 freertos
a53ss1-0 freertos
a53ss1-1 freertos
a53ss0-0 freertos-smp
c75ss0-0 freertos
r5fss0-0 nortos
r5fss0-0 freertos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
ti-c7000
Boards am62dx-evm
Example folder examples/hello_world/

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

Hello World!

FreeRTOS-AMP Sample Output

Attention
Output from a53ss0-1, a53ss1-0 and a53ss1-1 cores are log to the Shared memory, can be viewed via a53ss0-0 on which log reader is enabled

Shown below is a sample output on UART0 console when the application is run,

Hello World! from a53_core0
[a530-1] 0.002216s : Hello World! from a53_core1
[a531-0] 0.002184s : Hello World! from a53_core2
[a531-1] 0.002050s : Hello World! from a53_core3