AM62D FreeRTOS SDK  12.00.00
UART Echo DMA

Introduction

This example demonstrates the UART RX and TX operation in blocking, DMA-PKTDMA mode of operation. This example receives 8 characters and echos back the same. The application ends when the user types 8 characters.

Supported Combinations

Parameter Value
CPU + OS a53ss0-0 nortos
a53ss0-0 freertos
c75ss0-0 freertos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
ti-c7000
Board am62dx-evm
Example folder examples/drivers/uart/uart_echo_dma

Steps to Run the Example

See Also

UART

Sample Output

Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console. In UART console you need to enter 8 characters.

UART Console:

This is uart echo test DMA blocking mode
Receives 8 characters then echo's back. Please input..
12345678
All tests have passed!!