AM62D FreeRTOS SDK  12.00.00
SA3UL SHA Test

Introduction

This example demonstrates the how to generate SHA hash using SA3UL module.

Supported Combinations

Steps to Run the Example

See Also

SA3UL

Sample Output

Shown below is a sample output when the application is run.

CCS Console:

[CRYPTO] SHA example started ...
[CRYPTO] SHA-512 example completed!!
[CRYPTO] SHA-256 example completed!!
All tests have passed!!