AM62D FreeRTOS SDK  12.00.00
SA3UL Random Number Generator Test

Introduction

This example demonstrates the Random number generation using SA3UL module.

Supported Combinations

Steps to Run the Example

See Also

SA3UL

Sample Output

Shown below is a sample output when the application is run.

CCS Console:

All tests have passed!!
[SA3UL] Sa3ul Rng example started ...
[SA3UL] Sa3ul Rng output word 1 -- 0x3704DD0A
[SA3UL] Sa3ul Rng output word 2 -- 0x68719DEA
[SA3UL] Sa3ul Rng output word 3 -- 0x3A2733EE
[SA3UL] Sa3ul Rng output word 4 -- 0x943F007E
[SA3UL] Sa3ul Rng output word 1 -- 0xCE83C20D
[SA3UL] Sa3ul Rng output word 2 -- 0xAEB445B0
[SA3UL] Sa3ul Rng output word 3 -- 0xE052FEC9
[SA3UL] Sa3ul Rng output word 4 -- 0x713231C3
[SA3UL] Sa3ul Rng output word 1 -- 0xD5CF553B
[SA3UL] Sa3ul Rng output word 2 -- 0x1AB11E5F
[SA3UL] Sa3ul Rng output word 3 -- 0x25163494
[SA3UL] Sa3ul Rng output word 4 -- 0x5CD0432F
[SA3UL] Sa3ul Rng output word 1 -- 0x8372B743
[SA3UL] Sa3ul Rng output word 2 -- 0x75AA97AC
[SA3UL] Sa3ul Rng output word 3 -- 0x59F277C7
[SA3UL] Sa3ul Rng output word 4 -- 0x8DFC768C
[SA3UL] Sa3ul Rng output word 1 -- 0xAF3B154C
[SA3UL] Sa3ul Rng output word 2 -- 0x3A93F540
[SA3UL] Sa3ul Rng output word 3 -- 0xC3174A84
[SA3UL] Sa3ul Rng output word 4 -- 0xA361D316
[SA3UL] Sa3ul Rng example completed!!
All tests have passed!!