AM62D FreeRTOS SDK  12.00.00
PMU Multievent

Introduction

This example demonstrates the usage of the R5 PMU Driver. The PMU supports three event counters in additional to the cycle counter. So in total we could profile a block of code / or a function for four metrics. The cycle counter is a dedicated counter, but the other three are configurable for various PMU events. In this example, we configure the counters to count these events:

  • ICache Miss
  • DCache Miss
  • DCache Access

After profiling the above events, we can change events to following events to count these events:

  • Branch instructions executed
  • Branch Misses
  • Instructions executed

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
mcu-r5fss0-0 freertos
Toolchain ti-arm-clang
Board am62dx-evm
Example folder examples/drivers/pmu/pmu_multievent

Steps to Run the Example

See Also

UART

Sample Output

Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console.

UART Console:

[PMU Multievent] Starting...
Icache miss, Dcache access, Dcache miss...
CRC Value: 37090
Profile Point: Fxn2
Cycle Count: 94343
ICache Miss Count: 37
DCache Access Count: 5042
DCache Miss Count: 25
Profile Point: Fxn1
Cycle Count: 4018
ICache Miss Count: 6
DCache Access Count: 1041
DCache Miss Count: 0
Profile Point: Fxn2
Cycle Count: 94343
ICache Miss Count: 37
DCache Access Count: 5042
DCache Miss Count: 25
Profile Point: Fxn3
Cycle Count: 10361
ICache Miss Count: 5
DCache Access Count: 2323
DCache Miss Count: 0
Branch instructions executed, Branch Misses, Instructions executed...
CRC Value: 37090
Profile Point: Fxn2
Cycle Count: 92352
Branch instructions executed Count: 2709
Branch Misses Count: 347
Instructions executed Count: 15069
Profile Point: Fxn1
Cycle Count: 3844
Branch instructions executed Count: 531
Branch Misses Count: 15
Instructions executed Count: 3141
Profile Point: Fxn2
Cycle Count: 92352
Branch instructions executed Count: 2709
Branch Misses Count: 347
Instructions executed Count: 15069
Profile Point: Fxn3
Cycle Count: 10222
Branch instructions executed Count: 1349
Branch Misses Count: 132
Instructions executed Count: 8237
[PMU Multievent] Done...
All tests have passed!!