AM62D FreeRTOS SDK  12.00.00
MCSPI Loopback

Introduction

This example demonstrates the McSPI RX and TX operation configured in blocking, interrupt mode of operation.

This example sends a known data in the TX mode of length APP_MCSPI_MSGSIZE and then receives the same in RX mode. Internal pad level loopback mode is enabled to receive data. To enable internal pad level loopback mode, D0 pin is configured to both TX Enable as well as RX input pin in the SYSCFG.

When transfer is completed, TX and RX buffer data are compared. If data is matched, test result is passed otherwise failed.

To modify the example to use main domain SPI, refer Accessing main and wakeup domain peripherals from MCU domain

Supported Combinations

Parameter Value
CPU + OS a53ss0-0 nortos
a53ss0-0 freertos
c75ss0-0 freertos
mcu-r5fss0-0 nortos
mcu-r5fss0-0 freertos
Toolchain ti-arm-clang
arm.gnu.aarch64-none
ti-c7000
Boards am62dx-evm
Example folder examples/drivers/mcspi/mcspi_loopback
Parameter Value
CPU + OS a53ss0-0 nortos
mcu-r5fss0-0 freertos
mcu-r5fss0-0 nortos
Toolchain arm.gnu.aarch64-none
ti-arm-clang
Board am62dx-evm
Example folder examples/drivers/mcspi/mcspi_loopback

Steps to Run the Example

See Also

MCSPI

Sample Output

Shown below is a sample output when the application is run,

[MCSPI] Loopback example started ...
All tests have passed!!