AM62D FreeRTOS SDK  12.00.00
DMA Utils autoincrement compression example

Introduction

Demostrates a simple example of auto increment DMA to allow DSP to operate a function on internal memory and transfer back the result with compression.

The application runs on C7x core. UDMA is configured for UTC/DRU mode.

Supported Combinations

Parameter Value
CPU + OS c75ss0-0 freertos
Toolchain ti-arm-clang
Boards am62dx-evm
Example folder examples/dmautils/dmautils_autoinc_compression/

Steps to Run the Example

Sample Output

Shown below is a sample output when the benchmark application is run,

c7x core:

width : 1024
height : 128
Tensor Filled
Tensor Compressed
Tensor Un-compressed
DMAUtils Compression TestCase 0, PASSED
width : 1024
height : 128
Tensor Filled
Tensor Compressed
Tensor Un-compressed
DMAUtils Compression TestCase 1, PASSED
width : 1024
height : 128
Tensor Filled
Tensor Compressed
Tensor Un-compressed
DMAUtils Compression TestCase 2, PASSED
width : 1024
height : 128
Tensor Filled
Tensor Compressed
Tensor Un-compressed
DMAUtils Compression TestCase 3, PASSED
width : 1024
height : 128
Tensor Filled
Tensor Compressed
Tensor Un-compressed
DMAUtils Compression TestCase 4, PASSED
width : 1024
height : 128
Tensor Filled
Tensor Compressed
Tensor Un-compressed
DMAUtils Compression TestCase 0, PASSED
All tests have passed!!