AM62D FreeRTOS SDK  12.00.00
Ethernet Firmware

Introduction

This Ethernet Firmware example demonstrates ability to perform traffic steering from CPSW to multiple cores. This uses hardware capabilities of CPSW to direct unicast traffic, and a shared memory based layer to send multicast and broadcast traffic.

Ethernet Firmware server is the application which owns the CPSW peripheral, and controls the behaviour. Ethernet firmware clients are the applications which are running on different cores, which send requests to ethernet firmware server based on their requirements.

This demo showcases the integration of AVB functionality with Ethernet Firmware. The configuration utilizes two boards in complementary roles, one acting as AVTP Talker and the other as an AVTP Listener, while simultaneously supporting MAC-only mode on port 2 for other network traffic.

Port Configuration in the example:
MAC Port 1: Configured in switch mode, used for AVB audio streaming between boards.
MAC Port 2: Configured in MAC-only mode, allowing direct traffic to the host port without packet switching.

Note
This is in work-in-progress state currently, and complete feature list and functionality will be updates as functional validation progresses.
Attention
For more information, please refer to the link https://software-dl.ti.com/jacinto7/esd/processor-sdk-rtos-j784s4/latest/exports/docs/ethfw/docs/user_guide/ethfw_c_ug_top.html

Supported Combinations

Ethernet Firmware Server

Parameter Value
CPU + OS r5fss0-0_freertos (Server app)
c75ss0-0_freertos (Audio data sink)
Toolchain ti-arm-clang
Board am62dx-evm
Example folder source/networking/ethfw/apps/app_remoteswitchcfg_server/sitara/avb_audio_source
source/networking/ethfw/apps/app_remoteswitchcfg_server/sitara/avb_audio_sink

Ethernet Firmware Client

Parameter Value
CPU + OS mcu-r5fss0-0_freertos
Toolchain ti-arm-clang
Board am62dx-evm
Example folder source/networking/ethfw/apps/app_remoteswitchcfg_client/sitara/

Other Clients supported

Client Env Supported Core + OS
MCAL Client Not supported
Linux Client Not supported

Steps to Run the Example

Prerequisites

  • Two am62dx-evm boards
  • CAT6 Ethernet cable

Build the example

Attention
The out-of-box CPSW resource allocation needs to be modified to enable ethernet firmware functionality.
Follow the steps mentioned in CPSW resource partitioning for Ethernet Firmware before running the example.
  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

HW Setup

  • Connect one end of the CAT6 cable to MAC port 1 of DUT 1 and the other end to MAC port 1 of DUT 2. Optionally, connect MAC Port 2 of each board to external networks if desired.

Run the example

Attention
If you need to reload and run again, a CPU power-cycle is MUST.
Note
CCS loading is not supported for any core. Applications are tested with OSPI boot mode
  • Load R5 Server Talker binary to DUT-1 (Talker) and R5 Server Listener binary to DUT-2 via OSPI boot mode.
  • Load other binaries via SBL flow or U-boot flow.
  • You will see logs in the UART terminal as shown in the next section.
  • The prints will indicate the IP address acquired by clients against their corresponding MAC addresses

Sample output

Sample Ethernet Firmware Server with AVTP talker logs

=======================================================
CPSW Ethernet Firmware
=======================================================
Open MAC port 1
EnetPhy_bindDriver:1942
Open MAC port 2
EnetPhy_bindDriver:1942
PHY 3 is alive
ETHFW: Shared multicasts:
ETHFW: 01:00:5e:00:00:01
ETHFW: 01:00:5e:00:00:fb
ETHFW: 01:00:5e:00:00:fc
ETHFW: 33:33:00:00:00:01
ETHFW: 33:33:ff:1d:92:c2
ETHFW: 01:80:c2:00:00:00
ETHFW: 01:80:c2:00:00:03
ETHFW: Reserved multicasts:
ETHFW: 01:80:c2:00:00:0e
ETHFW: 01:1b:19:00:00:00
ETHFW: VLAN 1024 member=0x3 virtMember=0xe000000 regMcastFlood=0x3 unregMcastFlood=0x3 untag=0x0
ETHFW: 1 VLAN entries added in ALE table
ETHFW: PPS via GenF is not supported for this SoC
ETHFW Version : 0.05.00
ETHFW Build Date: Nov 27, 2025
ETHFW Build Time: 16:41:29
ETHFW Commit SHA:
ETHFW: Virtual port configuration:
ETHFW: CpswProxyServer: initialization completed (core: mcu2_0)
unibase-1.1.4
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
Host MAC address-0 : 70:ff:76:1d:ec:f2
ETHFW: Enable gPTP on MAC port 1 (tilld1)
[LWIPIF_LWIP_IC] Interface started successfully
[LWIPIF_LWIP_IC] NETIF INIT SUCCESS
[LWIPIF_LWIP_IC] Interface started successfully
[LWIPIF_LWIP_IC] NETIF INIT SUCCESS
[LWIPIF_LWIP] Enet has been started successfully
Added interface 'br3', IP is 0.0.0.0
ETHFW: TimeSync PTP enabled
ETHFW: ATTACH | C2S | core=0 endpt=36 virtPort=26
ETHFW: ATTACH | S2C | token=2600 rxMtu=1522 features=3
ETHFW: ATTACH | C2S | core=0 endpt=36 virtPort=2
ETHFW: ATTACH | S2C | token=200 rxMtu=1522 features=1
ETHFW: ALLOC_TX | C2S | core=0 endpt=36 token=2600
ETHFW: ALLOC_TX | S2C | txPsil=0xc603 status=0
ETHFW: ALLOC_RX | C2S | core=0 endpt=36 token=2600
ETHFW: ALLOC_RX | S2C | flow=20,5 rxPsil=0x4600 status=0
ETHFW: ALLOC_MAC | C2S | core=0 endpt=36 token=2600
ETHFW: ALLOC_MAC | S2C | macAddr=70:ff:76:1d:ec:e7 status=0
tilld1: has mac: 70:FF:76:1D:EC:F2
cb_lld_task_create: Uniconf Task stack_size=16384
cb_rawsock_open:combase-1.1.3
cb_rawsock_open:dmaTxChId=-1 numRxChaCPSW_ALE_IOCTL_ADD_VLAN: 110
CPSW_ALE_IOCTL_ADD_VLAN: 110
ETHFW: REGISTER_MAC | C2S | core=0 endpt=36 token=2600 macAdd=70:ff:76:1d:ec:e7 flowIdx=20,5
Cpsw_internalIoctl_handler_ENET_IOCTL_REGISTER_DSTMAC_RX_FLOW:432
ETHFW: REGISTER_MAC | S2C | status=0
cb_lld_task_create: gPTP Task stack_size=16384
cb_lld_task_create: autoAmpApp_TxTask stack_size=16384
cb_lld_task_create: aETHFW: ALLOC_MAC | C2S | core=0 endpt=36 token=200
ETHFW: ALLOC_MAC | S2C | macAddr=70:ff:76:1d:ec:e1 status=0
r GPTP ready!!
Waiting for GPTP ready!!
cbl_query_response:tilld1 link DOWN !!!!
gptpman_run:max_domains=1, max_ports=1
cb_rawsock_open:combase-1.1.3
IETHFW: REGISTER_MAC | C2S | core=0 endpt=36 token=200 macAdd=70:ff:76:1d:ec:e1 flowIdx=20,5
ETHFW: REGISTER_MAC | S2C | status=0
=1 dmaRxChId=2 nTxPkts=16 nRxPkts=16 pktSize=1536
rxChId 2 has owner dmaRxShared 0
dev:tilld1 open success
gptpnet_init:supportRtNotice=0 tout_interval=125000000Ns
IEEE1588-2019 performance monitoring disabled.
pp_glb_init: use-mgt-log-gptp-cap-interval=0
current-log-gptp-cap-interval=3 initial-log-gptp-cap-interval=3
pp_glb_inent-log-gptp-cap-interval=3 initial-log-gptp-cap-interval=3
static_domains_init: instance=0, di=0, pi=1, currentToutIntervalNs=125000000
syncIntervalNs=125000000, announceInterveInterval=0
onenet_activate:tilld1 status=0, duplex=1, speed=0Mbps
GPTP_MEDIUM_ALLOC: fragsize=16 fragused/fragnum=630/944 (66)
GPTP_SMALL_ALLOC: fragsize=4 fraguseagsize=8 fragused/fragnum=1115/2032 (54)
domainIndex=0, GM changed old=00:00:00:00:00:00:00:00, new=70:FF:76:FF:FE:1D:EC:F2
GPTP ready!!t_gmsync:gptpInstanceIndex=INF:def05:
gptpmasterclock_init: tsn_gptp-1.2.3, ref_counter=1
avtpc_init: l2-1.2.3
cb_rawsock_open:combase-1.1.3
cb_rawsock_open:dmaTxChId6 pktSize=1536
avtpc_direct_setup:direct is set: tx=1, rx=0
conl2_avtpc_talker_init:avtp connected
avtpc_init: l2-1.2.3
cb_rawsock_open:combase-1.1.3
s=1 dmaRxChId=3 nTxPkts=16 nRxPkts=16 pktSize=1536
avtpc_direct_setup:direct is set: tx=1, rx=0
conl2_avtpc_talker_init:avtp connected
Starting All Talker in one sptpmasterclock_init: tsn_gptp-1.2.3, ref_counter=2
Monitor rxstream[7]=0
Monitor rxstream[7]=255
Monitor rxstream[7]=255
Monitor rxstream[7]=255
INF:gter=3
avtpc_init: l2-1.2.3
cb_rawsock_open:combase-1.1.3
cb_rawsock_open:dmaTxChId=2 numRxChannels=1 dmaRxChId=3 nTxPkts=16 nRxPkts=16 pktSize=1536
rxCt_setup:go ahead without the pipe, it may make problems for closing
ll_avtpe_receive_data: enable Rx Zero-Copy
cb_lld_task_create: avtpcrx_tilld1 stack_size=8192
avtpc_direct_setup:direct is set: tx=0, rx=1
[RX=0] Packet Count: 0
[RX=0] Packet Count: 0
Cpsw_handleLinkUp:1423
MAC Port 2: link up
[0]Network Link UP Event
Cpsw_handleLinkUp:1423
MAC Port 1: link up
cbl_query_response:tilld1: link UP, speed=1000, duplex=1 !!!! (148us since link change event)
index=1 speed=1000, duplex=full
waiting_for_pdelay_interval_timer_proc:portIndex=1, sourcePortIdentity=70:FF:76:FF:FE:1D:EC:F3, thisClock=70:FF:76:FF:FE:for_pdelay_interval_timer_proc:portIndex=1, not asCapable
set neighborGptpCapable, domainIndex=0, portIndex=1 wtout=24000000000
[RX=0] Packet Count: 745
waiting_for_pdelay_interval_timer_proc:set asCapableAcrossDomains, portIndex=1
set asCapable for domainIndex=0, portIndex=1
gm_stable:gm_unstable_proc:domainIndex=0
gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=1
setSyncTwoStep_txSync:domainIndex=0, portIndex=1, sync gap=4875msec, tsync_ts_threshold=175msec
[RX=0] Packet Count: 1745mainIndex=0, portIndex=1,
[RX=0] Packet Count: 2745
[RX=0] Packet Count: 3745
[RX=0] Packet Count: 4745
[RX=0] Packet Count: 5744
[RX=0] Packet Count: 6744
[RX=0] Packet Count: 7744

Sample Ethernet Firmware Server with AVTP Listener logs

=======================================================
CPSW Ethernet Firmware
=======================================================
Open MAC port 1
EnetPhy_bindDriver:1942
Open MAC port 2
EnetPhy_bindDriver:1942
PHY 3 is alive
ETHFW: Shared multicasts:
ETHFW: 01:00:5e:00:00:01
ETHFW: 01:00:5e:00:00:fb
ETHFW: 01:00:5e:00:00:fc
ETHFW: 33:33:00:00:00:01
ETHFW: 33:33:ff:1d:92:c2
ETHFW: 01:80:c2:00:00:00
ETHFW: 01:80:c2:00:00:03
ETHFW: Reserved multicasts:
ETHFW: 01:80:c2:00:00:0e
ETHFW: 01:1b:19:00:00:00
ETHFW: VLAN 1024 member=0x3 virtMember=0xe000000 regMcastFlood=0x3 unregMcastFlood=0x3 untag=0x0
ETHFW: 1 VLAN entries added in ALE table
ETHFW: PPS via GenF is not supported for this SoC
ETHFW Version : 0.05.00
ETHFW Build Date: Nov 27, 2025
ETHFW Build Time: 16:41:29
ETHFW Commit SHA:
ETHFW: Virtual port configuration:
ETHFW: CpswProxyServer: initialization completed (core: mcu2_0)
unibase-1.1.4
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
Host MAC address-0 : 70:ff:76:1d:ec:f3
ETHFW: Enable gPTP on MAC port 1 (tilld1)
[LWIPIF_LWIP_IC] Interface started successfully
[LWIPIF_LWIP_IC] NETIF INIT SUCCESS
[LWIPIF_LWIP_IC] Interface started successfully
[LWIPIF_LWIP_IC] NETIF INIT SUCCESS
[LWIPIF_LWIP] Enet has been started successfully
Added interface 'br3', IP is 0.0.0.0
ETHFW: TimeSync PTP enabled
ETHFW: ATTACH | C2S | core=0 endpt=36 virtPort=26
ETHFW: ATTACH | S2C | token=2600 rxMtu=1522 features=3
ETHFW: ATTACH | C2S | core=0 endpt=36 virtPort=2
ETHFW: ATTACH | S2C | token=200 rxMtu=1522 features=1
ETHFW: ALLOC_TX | C2S | core=0 endpt=36 token=2600
ETHFW: ALLOC_TX | S2C | txPsil=0xc603 status=0
ETHFW: ALLOC_RX | C2S | core=0 endpt=36 token=2600
ETHFW: ALLOC_RX | S2C | flow=20,5 rxPsil=0x4600 status=0
ETHFW: ALLOC_MAC | C2S | core=0 endpt=36 token=2600
ETHFW: ALLOC_MAC | S2C | macAddr=70:ff:76:1d:ec:e9 status=0
tilld1: has mac: 70:FF:76:1D:EC:F3
cb_lld_task_create: Uniconf Task stack_size=16384
cb_rawsock_open:combase-1.1.3
cb_rawsock_open:dmaTxChId=-1 numRxChaCPSW_ALE_IOCTL_ADD_VLAN: 110
CPSW_ALE_IOCTL_ADD_VLAN: 110
ETHFW: REGISTER_MAC | C2S | core=0 endpt=36 token=2600 macAdd=70:ff:76:1d:ec:e9 flowIdx=20,5
Cpsw_internalIoctl_handler_ENET_IOCTL_REGISTER_DSTMAC_RX_FLOW:432
ETHFW: REGISTER_MAC | S2C | status=0
cb_lld_task_create: gPTP Task stack_size=16384
cb_lld_task_create: autoAmpApp_TxTask stack_size=16384
cb_lld_task_create: aETHFW: ALLOC_MAC | C2S | core=0 endpt=36 token=200
ETHFW: ALLOC_MAC | S2C | macAddr=70:ff:76:1d:ec:ea status=0
r GPTP ready!!
Waiting for GPTP ready!!
cbl_query_response:tilld1 link DOWN !!!!
gptpman_run:max_domains=1, max_ports=1
cb_rawsock_open:combase-1.1.3
IETHFW: REGISTER_MAC | C2S | core=0 endpt=36 token=200 macAdd=70:ff:76:1d:ec:ea flowIdx=20,5
ETHFW: REGISTER_MAC | S2C | status=0
=1 dmaRxChId=2 nTxPkts=16 nRxPkts=16 pktSize=1536
rxChId 2 has owner dmaRxShared 0
dev:tilld1 open success
gptpnet_init:supportRtNotice=0 tout_interval=125000000Ns
IEEE1588-2019 performance monitoring disabled.
pp_glb_init: use-mgt-log-gptp-cap-interval=0
current-log-gptp-cap-interval=3 initial-log-gptp-cap-interval=3
pp_glb_inent-log-gptp-cap-interval=3 initial-log-gptp-cap-interval=3
static_domains_init: instance=0, di=0, pi=1, currentToutIntervalNs=125000000
syncIntervalNs=125000000, announceInterveInterval=0
onenet_activate:tilld1 status=0, duplex=1, speed=0Mbps
GPTP_MEDIUM_ALLOC: fragsize=16 fragused/fragnum=630/944 (66)
GPTP_SMALL_ALLOC: fragsize=4 fraguseagsize=8 fragused/fragnum=1115/2032 (54)
domainIndex=0, GM changed old=00:00:00:00:00:00:00:00, new=70:FF:76:FF:FE:1D:EC:F3
GPTP ready!!t_gmsync:gptpInstanceIndex=INF:def05:
gptpmasterclock_init: tsn_gptp-1.2.3, ref_counter=1
avtpc_init: l2-1.2.3
cb_rawsock_open:combase-1.1.3
cb_rawsock_open:dmaTxChId6 pktSize=1536
avtpc_direct_setup:direct is set: tx=1, rx=0
conl2_avtpc_talker_init:avtp connected
Starting All Talker in one single threads
GPTP ready ref_counter=2
Monitor rxstream[7]=2
Monitor rxstream[7]=1
Monitor rxstream[7]=255
Monitor rxstream[7]=255
gptpmasterclock_init: tsn_gptp-1.
cb_rawsock_open:combase-1.1.3
cb_rawsock_open:dmaTxChId=2 numRxChannels=1 dmaRxChId=3 nTxPkts=16 nRxPkts=16 pktSize=1536
rxChId 3 has owner dmaRxShared 0
INF:defmay make problems for closing
ll_avtpe_receive_data: enable Rx Zero-Copy
cb_lld_task_create: avtpcrx_tilld1 stack_size=8192
rxethernet_setup:rxethernet_setup is do=0, rx=1
[RX=2] Packet Count: 0
[RX=1] Packet Count: 0
[RX=2] Packet Count: 0
[RX=1] Packet Count: 0
Cpsw_handleLinkUp:1423
MAC Port 2: link up
[0]Network Link UP Event
Cpsw_handleLinkUp:1423
MAC Port 1: link up
cbl_query_response:tilld1: link UP, speed=1000, duplex=1 !!!! (770us since link change event)
index=1 speed=1000, duplex=full
set neighborGptpCapable, domainIndex=0, portIndex=1 wtout=24000000000
waiting_for_pdelay_interval_timer_proc:portIndex=1, sourcePortIdentity=70:FF:76:FF:FE:1DPropDelay=412
waiting_for_pdelay_interval_timer_proc:portIndex=1, not asCapable
[RX=2] Packet Count: 519
[RX=1] Packet Count: 64
waiting_for_pdelay_interval_timer_proc:set asCapableAcrossDomains, portIndex=1
set asCapable for domainIndex=0, portIndex=1
gm_stable:gm_unstable_proc:domainIndex=0
gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=1
gm_stable:gm_unstable_proc:domainIndex=0
setSyncTwoStep_txSync:domainIndex=0, portIndex=1, sync gap=8125msec, tsync_ts_threshold=175msec
[RX=2] Packet Count: 1519mainIndex=0, portIndex=1,
[RX=1] Packet Count: 189
domainIndex=0, GM changed old=70:FF:76:FF:FE:1D:EC:F3, new=70:FF:76:FF:FE:1D:EC:F2
gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=0
INF:gptp:00=0
gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=1
set_phase_offsetGM:domainIndex=0, New adjustment(New GM?)
set_phase_offsetGM:domainIndex=0, stable
[RX=2] Packet Count: 2519
[RX=1] Packet Count: 314
[RX=2] Packet Count: 3519
[RX=1] Packet Count: 439
[RX=2] Packet Count: 4519
[RX=1] Packet Count: 564
[RX=2] Packet Count: 5519
[RX=1] Packet Count: 689
domainIndex=0, clock_master_sync_receive:stable rate
gptpclock_set_gmsync:gptpInstanceIndex=0, domainIndex=0, gmstate=2
[RX=2] Packet Count: 6519domain
[RX=1] Packet Count: 814
[RX=2] Packet Count: 7519
[RX=1] Packet Count: 939

MCU-R5 Client Application logs

CpswProxy: Local cmd endpt 36, notify endpt 30
CpswProxy: ETHFW services found at core 1 endpts 34 (ti.ethfw.ethdevice) and 24 (ti.ethfw.notifyservice)
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
CpswProxy: ATTACH | C2S | virtPort=26
CpswProxy: ATTACH | S2C | token=2600 rxMtu=1522 features=3 numTxCh=1 numRxFlow=1 status=0
CpswProxy: ATTACH | C2S | virtPort=2
CpswProxy: ATTACH | S2C | token=200 rxMtu=1522 features=1 numTxCh=1 numRxFlow=1 status=0
CpswProxy: ALLOC_TX | C2S | token=2600 chRelPri=0
CpswProxy: ALLOC_TX | S2C | token=2600 txPsil=0xc603 chRelPri=0 status=0
CpswProxy: ALLOC_RX | C2S | token=2600
CpswProxy: ALLOC_RX | S2C | token=2600 flow=20,5 rxPsil=0x4600 status=0
CpswProxy: ALLOC_MAC | C2S | token=2600
CpswProxy: ALLOC_MAC | S2C | token=2600 macAddr=70:ff:76:1d:ec:e7 status=0
CpswProxy: REGISTER_MAC | C2S | token=2600 flowIdx=20,5
CpswProxy: REGISTER_MAC | S2C | token=2600 status=0
CpswProxy: ALLOC_MAC | C2S | token=200
CpswProxy: ALLOC_MAC | S2C | token=200 macAddr=70:ff:76:1d:ec:e1 status=0
CpswProxy: REGISTER_MAC | C2S | token=200 flowIdx=20,5
CpswProxy: REGISTER_MAC | S2C | token=200 status=0
Host MAC address : 70:ff:76:1d:ec:e7
[LWIPIF_LWIP] Enet has been started successfully
Added interface 'ti0', IP is 0.0.0.0
Starting lwIP, local interface IP is dhcp-enabled
[LWIPIF_LWIP] NETIF INIT SUCCESS
Added interface 'ti1', IP is 0.0.0.0
[0]Network Link UP Event
[1]Network Link UP Event
Added interface 'ti1', IP is 192.168.1.48

MAC-only port

Ethernet Firmware enables MAC-only mode on MAC port 2 for AM62Dx, this allows all incoming traffic from MAC port 2 to be transferred only to the host port. This effectively excludes the MAC port from rest of packet switching in the CPSW switch.
The key concepts of a system with MAC-only mode enabled are as follows:

  • Logical switch ports - Defined based on packet header match criteria, typically created based on destination MAC address, VLAN IDs, etc. Two possible types:
    • Local Switch port - owned exclusively by Ethernet Firmware.
    • Virtual Switch port - owned by remote clients.
  • Logical MAC-only ports - Defined with 1-to-1 correspondence to physical ports (port configured in MAC-only mode), owned by remote clients.
    • Virtual MAC port - owned by remote clients.

The default port configuration for AM62Dx is shown below:

See Also

Ethernet And Networking