AM62D FreeRTOS SDK  12.00.00
Ethernet AVB Stack - API and Integration Guide

Pre-requisites

Reader are expected to have basic knowledge on below IEEE specifications:

  • Standard ethernet (IEEE 802.1)
  • Timing and Synchronization for Time-Sensitive Applications - gPTP (IEEE 802.1AS-2020)
  • Forwarding and Queuing Enhancements for Time-Sensitive Streams (IEEE 802.1Qav)
  • Enhancements for Scheduled Traffic (IEEE 802.1Qbv)
  • Frame Preemption (IEEE 802.1Qbu)
  • IEEE Standard for a Transport Protocol for Time-Sensitive Applications in Bridged Local Area Networks (IEEE Std 1722™-2016)

Introduction

This guide is intended to enhance user's understanding of the AVB stack and provide guidance on how to seamlessly integrate AVB modules into their own applications.

Demo and Examples

Ethernet AVTP Example

TSN Stack

Compilation

The compilation of library is similar with Ethernet TSN and gPTP Stack - API and Integration Guide.

Modules

The TSN Stack library is composed of the following source modules:

Module Name lcoation Description
Unibase <${SDK_INSTALL_PATH}>/source/networking/tsn/tsn_unibase Universal utility libraries that are platform-independent
Combase <${SDK_INSTALL_PATH}>/source/networking/tsn/tsn_combase Communication utility libraries that provide support for functions like sockets, mutexes, and semaphores
Uniconf <${SDK_INSTALL_PATH}>/source/networking/tsn/tsn_uniconf Universal configuration daemon for Yang, provides APIs for developing a client application which retreives/writes yang parameters from/to database
gPTP <${SDK_INSTALL_PATH}>/source/networking/tsn/tsn_gptp Implementation of the IEEE 802.1 AS gptp protocol
l2/conl2 <${SDK_INSTALL_PATH}>/source/networking/tsn/tsn-stack/eval_lib The evaluation library which implements of the IEEE Std 1722™-2016 AVTP
yangemb <${SDK_INSTALL_PATH}>/source/networking/tsn/license_lib YangDB 1 hour limitted access for AVB Applications.

Stack Initialization

Refer Stack Initialization section

Logging

Refer Logging section

Starting uniconf and gPtp and avtp applications

Refer Starting uniconf and gPTP section.

This function will start:

  • The uniconf task as 1st priority task to be init
  • Initial uniconf DB after uniconf is finished by uniconf runtime config or yang config file.
  • After uniconf and DB initialization is finished, gptp task and avtp task are able to start

Applications Deinitialization

Refer TSN Deinitialization section

Integration

Source integration

Refer Source integration section

Uniconf configuration

Refer Uniconf configuration section

Licensing library

There is yangemb-freertos.am62dx.r5f.ti-arm-clang.lib located under <${SDK_INSTALL_PATH}>/source/networking/tsn/tsn-stack/license_lib, which must be added to all tsn-stack application's makefile.

Add <${SDK_INSTALL_PATH}>/source/networking/tsn/tsn-stack/license_lib to LIBS_PATH_common and yangemb lib file to LIBS_common flags.

The licensing library will Prevent all avtp applications running after 1 hour.

GPTP configuration parameters

Refer gPTP Yang Config Parameters section

AVTP configuration parameters

AVTP Applications list

App location Description
aafpcmlistener_app <${SDK_INSTALL_PATH}>/source/networking/enet/core/examples/tsn/aafpcmlistener_app AVTP AAF PCM Listener Example Application
aafpcmtalker_app <${SDK_INSTALL_PATH}>/source/networking/enet/core/examples/tsn/aafpcmtalker_app AVTP AAF PCM Talker Example Application
aes3_aaflistener_app <${SDK_INSTALL_PATH}>/source/networking/enet/core/examples/tsn/aes3_aaf/aes3_aaflistener_app/ AVTP AES3 format Listener Example Application
aes3_aaftalker_app <${SDK_INSTALL_PATH}>/source/networking/enet/core/examples/tsn/aes3_aaf/aes3_aaftalker_app/ AVTP AES3 format Talker Example Application

Configuration parameters

Refer to <${SDK_INSTALL_PATH}>/source/networking/enet/core/examples/tsn/avtp_init.c, the avtp talker/listener can only be actived with following definitions in project files.

  • Use #define AAF_PCM_ENABLED=1 to enable aaf pcm task. This has to be enabled for both AAF PCM Talker and Listener.
  • Use #define AAF_PCM_LISTENER_ENABLE=1 to enable aap pcm listener app

By default, aafpcmtalker_app and aafpcmlistener are configured to send and receive one stream with stream ID 00:01:02:03:04:05:00:00

See Also

Ethernet And Networking