|
AM62Ax MCU+ SDK
11.01.00
|
|
Go to the documentation of this file.
66 #define UDMA_RM_RES_ID_INVALID ((uint32_t) 0xFFFF0005U)
69 #define UDMA_RM_SHARED_RES_CNT_MIN ((uint32_t) 0xFFFF0006U)
72 #define UDMA_RM_SHARED_RES_CNT_REST ((uint32_t) 0xFFFF0007U)
227 #if (UDMA_NUM_UTC_INSTANCE > 0)
236 #if (UDMA_NUM_MAPPED_TX_GROUP > 0)
245 #if (UDMA_NUM_MAPPED_RX_GROUP > 0)
254 #if ((UDMA_NUM_MAPPED_TX_GROUP + UDMA_NUM_MAPPED_RX_GROUP) > 0)
uint32_t numGlobalEvent
Definition: udma_rm.h:276
#define UDMA_RM_SHARED_RES_MAX_INST
Maximum no.of instances to split a shared resource. This should be max(UDMA_NUM_CORE,...
Definition: am62ax/udma_soc.h:386
uint32_t numBlkCopyCh
Definition: udma_rm.h:187
uint32_t resId
Definition: udma_rm.h:83
uint32_t startFreeRing
Definition: udma_rm.h:268
uint32_t startTxCh
Definition: udma_rm.h:203
uint32_t startTxHcCh
Definition: udma_rm.h:197
uint32_t startResrvCnt
Definition: udma_rm.h:85
uint32_t startBlkCopyCh
Definition: udma_rm.h:185
uint32_t startVintr
Definition: udma_rm.h:279
uint32_t startC7xCoreIntr
Definition: udma_rm.h:289
uint32_t numFreeFlow
Definition: udma_rm.h:265
UDMA resource manager init parameters.
Definition: udma_rm.h:172
uint32_t numFreeRing
Definition: udma_rm.h:270
uint32_t numBlkCopyHcCh
Definition: udma_rm.h:182
uint32_t startBlkCopyUhcCh
Definition: udma_rm.h:173
uint32_t startRxHcCh
Definition: udma_rm.h:215
uint32_t startIrIntr
Definition: udma_rm.h:284
uint32_t numTxCh
Definition: udma_rm.h:205
uint32_t startTxUhcCh
Definition: udma_rm.h:191
uint32_t numRxUhcCh
Definition: udma_rm.h:212
Udma_RmSharedResPrms * Udma_rmGetSharedResPrms(uint32_t instId, uint32_t resId)
Returns the RM Shared Resource default parameters structure for the requested resource....
#define UDMA_NUM_MAPPED_RX_GROUP
Number of Mapped RX Group.
Definition: am62ax/udma_soc.h:168
uint32_t startGlobalEvent
Definition: udma_rm.h:274
uint32_t endResrvCnt
Definition: udma_rm.h:88
#define UDMA_NUM_UTC_INSTANCE
Number of UTC instance.
Definition: am62ax/udma_soc.h:209
uint32_t startRxUhcCh
Definition: udma_rm.h:209
uint32_t numTxUhcCh
Definition: udma_rm.h:194
UDMA resource manager shared resource parameters.
Definition: udma_rm.h:82
uint32_t numRxHcCh
Definition: udma_rm.h:218
#define UDMA_NUM_MAPPED_TX_GROUP
Number of Mapped TX Group.
Definition: am62ax/udma_soc.h:152
uint32_t numBlkCopyUhcCh
Definition: udma_rm.h:176
uint32_t startRxCh
Definition: udma_rm.h:221
uint32_t numTxHcCh
Definition: udma_rm.h:200
uint32_t numRxCh
Definition: udma_rm.h:223
uint32_t startFreeFlow
Definition: udma_rm.h:263
uint32_t numIrIntr
Definition: udma_rm.h:286
uint32_t startBlkCopyHcCh
Definition: udma_rm.h:179
uint32_t numInst
Definition: udma_rm.h:91
uint32_t minReq
Definition: udma_rm.h:97
uint32_t numVintr
Definition: udma_rm.h:281