![Logo](ti_logo.svg) |
AM62Ax MCU+ SDK
09.02.00
|
|
Go to the documentation of this file.
39 #ifndef SDL_MCRC_SOC_H_
40 #define SDL_MCRC_SOC_H_
46 #include <sdl/include/am62ax/sdlr_soc_baseaddress.h>
72 #define SDL_MCRC_INSTANCES 2u
@ MCRC64_0
Definition: sdl_mcrc_soc.h:63
SDL_MCRC_InstType
MCRC Instance supported.
Definition: sdl_mcrc_soc.h:60
@ MCU_MCRC64_0
Definition: sdl_mcrc_soc.h:61
bool SDL_MCRC_64bit_AtomicWriteSupport[SDL_MCRC_INSTANCES]
MCRC 64 bit Atomic write support.
#define SDL_MCRC_INSTANCES
MCRC instances supported by SOC.
Definition: sdl_mcrc_soc.h:72
@ SDL_MCRC_INVALID
Definition: sdl_mcrc_soc.h:65
int32_t SDL_MCRC_getBaseaddr(SDL_MCRC_InstType instance, uint32_t *baseAddr)
This API is used to get the base address of the instance.