Introduction
- SBL booting Linux from SD card (see SBL SD LINUX) is a secondary bootloader application that boots Linux on A53 core and RTOS/NORTOS application on R5, C7x cores.
- The bootloader makes use of 5 appimages
- A Linux appimage containing the Linux binaries (ATF, OPTEE, A53 SPL).
- tiboot3.bin with SBL SD, TIFS, BoardConfig
- Appimage for MCU R5
- Appimage for C75
- Appimage for DM R5
- The Linux appimage can be generated by using Linux Appimage Generator Tool
- The appimages will be copied to SD card, the SBL parses the appimages from the boot partition, loads and run the cores.
Bootflow for SBL booting linux from SD Card
- The bootflow for SBL booting Linux is as follows
Bootflow for SBL booting Linux
SD Card Partitioning
- SD card uses two partitions to boot Linux
- A boot partition
- tiboot3.bin
- mcu_r5_image
- dm_r5_image
- linux_a53_image
- c7x_image
- A ext4 partition in the user data area containing
- Linux Kernel image
- Linux DTB
- Linux file system
See Also