This example demonstrates High and Low priority events received from the MCU_ESM through the application-registered callback. It also shows routing and clearing of events to the MCU_SAFETY_ERRORn pin.
This example displays setting up ESM to
* Enable/Disable input events to the ESM module for each ESM instance * Registration of application callback for ESM error events for each ESM instance * Designating input events as high priority or low priority for each ESM instance * Designating direct pin routing to MCU_SAFETY_ERRORn pin for external monitor communication
| Use Case | Description |
|---|---|
| UC-0 | Configuration of High Priority ESM |
| UC-1 | Configuration of Config Priority ESM |
| UC-2 | Configuration of Low Priority ESM |
| Parameter | Value |
|---|---|
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am62ax-sk |
| Example folder | examples/sdl/mcu_esm0/ |
Shown below is a sample output when the application is run,