This example takes an aggregator index as input from the user and performs single bit error test for the corresponding aggregator. It involves the following steps:
The following aggregators can be tested using this example.
Aggregator Index | ECC Aggregator |
---|---|
0 | SDL_PSCSS0_SAM62A_MAIN_PSC_WRAP_ECC_AGGR |
1 | SDL_PSRAMECC0_PSRAM256X32E_ECC_AGGR |
2 | SDL_PSRAMECC1_PSRAM256X32E_ECC_AGGR |
3 | SDL_MSRAM_64K0_MSRAM2KX256E_ECC_AGGR |
4 | SDL_WKUP_ECC_AGGR1_SAM62A_DM_MCU_ECC_AGGR |
5 | SDL_DMASS1_DMSS_CSI_AM62A_ECCAGGR |
6 | SDL_MCU_MSRAM_256K1_MSRAM32KX64E_ECC_AGGR |
7 | SDL_WKUP_VTM0_K3VTM_N16FFC_ECCAGGR |
8 | SDL_FSS0_FSS_UL_OSPI0_OSPI_WRAP_ECC_AGGR |
9 | SDL_MCU_R5FSS0_PULSAR_ULS_CPU0_ECC_AGGR |
10 | SDL_CPSW0_CPSW_3GUSS_CORE_ECC_CPSW_ECC_AGGR |
11 | SDL_MCU_MSRAM_256K0_MSRAM32KX64E_ECC_AGGR |
12 | SDL_GICSS0_GIC500SS_1_4_ECC_AGGR |
13 | SDL_ECC_AGGR1_SAM62A_SEC_MCU_ECC_AGGR |
14 | SDL_DMASS0_DMSS_AM62A_ECCAGGR |
15 | SDL_CSI_RX_IF0_CSI_RX_IF_ECC_AGGR |
16 | SDL_MMCSD1_EMMCSD4SS_ECC_AGGR_RXMEM |
17 | SDL_MMCSD1_EMMCSD4SS_ECC_AGGR_TXMEM |
18 | SDL_MMCSD2_EMMCSD4SS_ECC_AGGR_RXMEM |
19 | SDL_MMCSD2_EMMCSD4SS_ECC_AGGR_TXMEM |
20 | SDL_MMCSD0_EMMCSD8SS_ECC_AGGR_TXMEM |
21 | SDL_MMCSD0_EMMCSD8SS_ECC_AGGR_RXMEM |
22 | SDL_MCU_ECC_AGGR0_SAM62A_MCU_MCU_ECC_AGGR |
23 | SDL_SA3_SS0_SA3SS_AM62A_DMSS_ECCAGGR |
24 | SDL_SA3_SS0_SA3SS_AM62A_SA_UL_ECC_AGGR |
25 | SDL_WKUP_ECC_AGGR2_SAM62A_WKUP_SAFE_ECC_AGGR |
26 | SDL_WKUP_R5FSS0_PULSAR_UL_CPU0_ECC_AGGR |
27 | SDL_SMS0_SMS_HSM_ECC |
28 | SDL_SMS0_SMS_TIFS_ECC |
29 | SDL_VPAC0_SAM62A_VPAC_WRAP_IVPAC_TOP_0_PAC_BASE_KSDW_ECC_AGGR |
30 | SDL_VPAC0_SAM62A_VPAC_WRAP_IVPAC_TOP_0_VPAC_LDC0_KSDW_ECC_AGGR |
31 | SDL_VPAC0_SAM62A_VPAC_WRAP_IVPAC_TOP_0_VPAC_VISS0_KSDW_ECC_AGGR |
32 | SDL_MCU_ECC_AGGR1_SAM62A_MCU_PULSAR_UL_ECC_AGGR |
33 | SDL_C7X256V0_SAM62A_C7XV_WRAP_ECC_AGGR |
34 | SDL_USB1_USB2SS_16FFC_USB2SS_CORE_ECC_AGGR |
35 | SDL_USB0_USB2SS_16FFC_USB2SS_CORE_ECC_AGGR |
36 | SDL_WKUP_PSRAMECC_8K0_PSRAM8KX32E_ECC_AGGR |
37 | SDL_PDMA0_SAM62_PDMA_SPI_ECCAGGR |
38 | SDL_WKUP_ECC_AGGR0_SAM62A_DM_DM_ECC_AGGR |
39 | SDL_PDMA1_SAM62_PDMA_UART_ECCAGGR |
40 | SDL_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR |
41 | SDL_COMPUTE_CLUSTER0_SAM62A_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE0 |
42 | SDL_COMPUTE_CLUSTER0_SAM62A_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE1 |
43 | SDL_COMPUTE_CLUSTER0_SAM62A_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE2 |
44 | SDL_COMPUTE_CLUSTER0_SAM62A_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE3 |
45 | SDL_COMPUTE_CLUSTER0_SAM62A_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_COREPAC |
46 | SDL_MCU_MCAN0_MCANSS_MSGMEM_WRAP_ECC_AGGR |
47 | SDL_MCU_MCAN1_MCANSS_MSGMEM_WRAP_ECC_AGGR |
48 | SDL_ECC_AGGR0_SAM62A_SEC_HSM_ECC_AGGR |
Parameter | Value |
---|---|
CPU + OS | mcu-r5fss0-0 nortos |
Toolchain | ti-arm-clang |
Board | am62ax-sk |
Example folder | examples/sdl/ecc_sec/ |
Shown below is a sample output when the application is run for a couple of aggregators,