This is an empty project provided for all cores present in the device. User can use this project to start their application by adding more SysConfig modules.
This application does driver and board init and just prints the pass string on the console. In case of the main core, the print is redirected to the UART console. For all other cores, CCS prints are used.
| Parameter | Value |
|---|---|
| CPU + OS | mcu-r5fss0-0 nortos |
| mcu-r5fss0-0 freertos | |
| c75ss0-0 freertos | |
| Toolchain | ti-arm-clang |
| Board | am62ax-sk |
| Example folder | examples/empty/ |
Shown below is a sample output when the application is run,