AM62Ax MCU+ SDK  09.02.00
UDMA SW Trigger

Introduction

UDMA SW trigger sample application performs 3D transfer using SW trigger method as below Loop N times (icnt2)

  • SW trigger CH 0 -> Triggers MSMC to Intermediate buffer
  • Wait for CH 0 icnt0 x icnt1 to complete
  • SW trigger Channel 1 -> Triggers Intermediate buffer to MSMC
  • Wait for CH 1 icnt0 x icnt1 to complete

Each loop transfers M (icnt0 x icnt1) bytes of data. MSMC size is M x N and intermediate buffer size is just M bytes. Intermediate buffer memory set to wrap around after M bytes of transfer.

Where,

  • M is icnt0 x icnt1 (UDMA_TEST_1D_SIZE x UDMA_TEST_2D_SIZE)
  • N is icnt2 = UDMA_TEST_3D_SIZE

Once the transfer it completes, it does cache operation for data coherency and compares the source and destination buffers for any data mismatch.

Supported Combinations

Parameter Value
CPU + OS a53ss0-0 nortos
Toolchain arm.gnu.aarch64-none
Board am62ax-sk
Example folder examples/drivers/udma/udma_sw_trigger

Steps to Run the Example

See Also

UDMA

Sample Output

Shown below is a sample output when the application is run,

[UDMA] SW Trigger application started ...
All tests have passed!!