UDMA chaining sample application performs a chain of block copy transfer using channel global trigger.
Channel 0 completion triggers Channel 1 transfer: CH0 -> CH1.
The application opens and configures two BCDMA channel using SysConfig.
The first channel doesn't user a global trigger and each channel triggers the next channel's global trigger through the channel's TR event register.
A channel's source buffer is previous channel's destination buffer. This ensures that chaining trigger works in a synchronized manner when the memory compare matches.
The transfer completion is based on last channel's DMA completion event. Once the transfer it completes, it does cache operation for data coherency and compares the source and destination buffers for any data mismatch.
| Parameter | Value |
|---|---|
| CPU + OS | a53ss0-0 nortos |
| Toolchain | arm.gnu.aarch64-none |
| Board | am62ax-sk |
| Example folder | examples/drivers/udma/udma_chaining |
Shown below is a sample output when the application is run,