AM62Ax MCU+ SDK  09.02.00
SBL OSPI NAND Multistage

Note
The load address of resource table for R5, M4 and A53 cores must be consistant with the address.

Introduction

This is a bootloader example, which shows an example of booting RTOS/NORTOS applications on DM R5, MCU R5 C75 and A53 cores.

The booting is done in 2 stages(2 bootloader applications).

  • The stage1 of the bootloader runs from the HSM RAM. It boots MCU R5 with RTOS/NORTOS application and initializes the DDR. Then it loads the stage2 of the bootloader to DDR and stats running it.
  • The stage2 of the bootloader boots RTOS/NORTOS on A53 and then self loads DM firmware on the DM R5.

The SBL uses 7 appimages

  • tiboot3.bin with SBL stage1, TIFS, BoardConfig
  • Appimage for SBL stage2
  • Appimage for MCU R5
  • Appimage for HSM M4
  • Appimage for C75
  • DM firmware appimage for DM R5
  • Appimage for A53

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am62ax-sk
Example folder examples/drivers/boot/sbl_ospi_nand_multistage

Steps to Run the Example

Build the example

Since this is a bootloader, the example will be run every time you boot an application using this example. It is run from a OSPI boot media unlike other examples which are usually loaded with CCS. Nevertheless, you can build this example like you do for the others using makefile or build it via CCS by importing as a project.

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Refer to the page Basic steps to flash files to flash this bootloader along with the application to boot.

Create HSM Appimage

  • Create a HSM Appimage
  • This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/HSMAppimageGen
  • Refer HSM Appimage Generator Tool for more details

Run the example

  • This example is the SBL which needs to be flashed on the EVM flash, along with sample application images for R5, M4 CPUs and A53 Appimage.
Note
For HS-SE device, use default_sbl_ospi_nand_hs.cfg as the cfg file.
For HS-FS device, use default_sbl_ospi_nand_hs_fs.cfg as the cfg file.
  • There is a default flash config file as shown below which flashes this SBL and the IPC RPMsg echo applications
      ${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/@VAR_SK_LP_BOARD_NAME_LOWER/default_sbl_ospi_nand.cfg
    
  • Make sure IPC rpms echo application is built before running the flash script. (see IPC RP Message Echo)
  • To flash to the EVM, refer to Flash an example application . Only when giving the flash config file, point to the default_sbl_ospi_nand.cfg shown above.
  • Example, assuming SDK is installed at C:/ti/mcu_plus_sdk and this example and IPC application is built using makefiles, and RTOS Appimage is already created, in Windows,
      cd C:/ti/mcu_plus_sdk/tools/boot
      python uart_uniflash.py -p COM13 --cfg=C:/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/@VAR_SK_LP_BOARD_NAME_LOWER/default_sbl_ospi_nand.cfg
    
  • If Linux PC is used, assuming SDK is installed at ~/ti/mcu_plus_sdk
      cd ~/ti/mcu_plus_sdk/tools/boot
      python uart_uniflash.py -p /dev/ttyUSB0 --cfg=~/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/@VAR_SK_LP_BOARD_NAME_LOWER/default_sbl_ospi_nand.cfg
    
  • This example is the SBL which needs to be flashed on the EVM flash, along with sample application images for DM R5, MCU R5, C75, HSM M4 CPUs and A53 Appimage.
    Note
    For HS-SE device, use default_sbl_ospi_nand_hs.cfg as the cfg file.
    For HS-FS device, use default_sbl_ospi_nand_hs_fs.cfg as the cfg file.
  • There is a default flash config file as shown below which flashes this SBL and the IPC RPMsg echo applications
      ${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/am62ax-sk/default_sbl_ospi_nand_hs_fs.cfg
    
  • Make sure IPC rpmsg echo application is built before running the flash script. (see IPC RP Message Echo)
Note
For IPC rpmsg echo, the resource table entity must be placed at the beginning of remoteproc memory section.
  • To flash to the EVM, refer to Flash an example application . Only when giving the flash config file, point to the default_sbl_ospi_nand_hs_fs.cfg shown above.
  • Example, assuming SDK is installed at C:/ti/mcu_plus_sdk and this example and IPC application is built using makefiles, and RTOS Appimage is already created, in Windows,
      cd C:/ti/mcu_plus_sdk/tools/boot
      python uart_uniflash.py -p COM13 --cfg=C:/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62ax-sk/default_sbl_ospi_nand_hs_fs.cfg
    
  • If Linux PC is used, assuming SDK is installed at ~/ti/mcu_plus_sdk
      cd ~/ti/mcu_plus_sdk/tools/boot
      python uart_uniflash.py -p /dev/ttyUSB0 --cfg=~/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62ax-sk/default_sbl_ospi_nand_hs_fs.cfg
    
  • Boot the EVM in OSPI NAND boot mode.

See Also

BOOTLOADER

Sample Output

After flashing and booting the EVM, you will see below output on the UART console (Complete log is not shown)

DMSC Firmware Version 9.1.8--v09.01.08 (Kool Koala)
DMSC Firmware revision 0x9
DMSC ABI revision 3.1

[BOOTLOADER_PROFILE] Boot Media       : FLASH
[BOOTLOADER_PROFILE] Boot Media Clock : 200.000 MHz
[BOOTLOADER_PROFILE] Boot Image Size  : 171 KB
[BOOTLOADER_PROFILE] Cores present    :
mcu-r5f0-0
r5f0-0
[BOOTLOADER PROFILE] System_init                      :      38003us
[BOOTLOADER PROFILE] Board_init                       :          0us
[BOOTLOADER PROFILE] Drivers_open                     :        193us
[BOOTLOADER PROFILE] Board_driversOpen                :         89us
[BOOTLOADER PROFILE] Sciclient Get Version            :       9909us
[BOOTLOADER PROFILE] App_loadImages                   :       3680us
[BOOTLOADER PROFILE] App_loadSelfcoreImage            :       8538us
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      60416us

Image loading done, switching to application ...
Starting MCU-r5f and 2nd stage bootloader
[BOOTLOADER_PROFILE] Boot Media       : FLASH
[BOOTLOADER_PROFILE] Boot Media Clock : 200.000 MHz
[BOOTLOADER_PROFILE] Boot Image Size  : 311 KB
[BOOTLOADER_PROFILE] Cores present    :
hsm-m4f0-0
r5f0-0
a530-0
c75ss0
[BOOTLOADER PROFILE] System_init                      :       1779us
[BOOTLOADER PROFILE] Board_init                       :          0us
[BOOTLOADER PROFILE] Drivers_open                     :        220us
[BOOTLOADER PROFILE] App_loadImages                   :       2326us
[BOOTLOADER PROFILE] App_loadSelfcoreImage            :       8543us
[BOOTLOADER PROFILE] App_loadA53Images                :       5045us
[BOOTLOADER PROFILE] App_loadDSPImages                :       6790us
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      24705us

Image loading done, switching to application ...
Starting RTOS/Baremetal applications
Hello World!