AM62Ax MCU+ SDK  09.02.00
SBL EMMC Multistage

Note
SBL EMMC RTOS/NORTOS boots from the boot partition 1 of eMMC. The appimage is flashed to the offsets in eMMC as configured using syscfg.
Attention
Care should be taken to ensure that the R5, M4 and A53 appimage flashed does NOT overwrite the binaries in eMMC.
Note
The load address of resource table for R5,M4 and A53 cores must be consistant with the address.

Introduction

This is a bootloader example, which shows an example of booting RTOS/NORTOS applications on R5,M4 and A53 cores from eMMC.

The booting is done in 2 stages(2 bootloader applications).

  • The stage1 of the bootloader runs from the HSM RAM. It boots MCU R5 with RTOS/NORTOS application and initializes the DDR. Then it loads the stage2 of the bootloader to DDR and stats running it.
  • The stage2 of the bootloader boots RTOS/NORTOS on A53, C75 and then self loads DM firmware on the DM R5.

The SBL uses 6 appimages

  • tiboot3.bin with SBL stage1, TIFS, BoardConfig
  • Appimage for SBL stage2
  • Appimage for MCU R5
  • Appimage for HSM M4
  • DM firmware appimage for DM R5
  • Appimage for A53
  • Appimage for C75

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am62ax-sk
Example folder examples/drivers/boot/sbl_emmc_multistage

Steps to Run the Example

Build the example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)

Create HSM Appimage

  • Create a HSM Appimage
  • This can be done by running the makefile at {SDK_INSTALL_PATH}/tools/boot/HSMAppimageGen
  • Refer HSM Appimage Generator Tool for more details

Run the example

  • This example is the SBL which needs to be flashed on the eMMC, along with sample application images for R5, M4 CPUs and A53 Appimage.
    Note
    Use default_sbl_emmc_hs.cfg when flashing to HS-SE devices
    Use default_sbl_emmc_hs_fs.cfg when flashing to HS-FS devices
  • There is a default flash config file as shown below which flashes this SBL and the IPC RPMsg echo applications
      ${SDK_INSTALL_PATH}/tools/boot/sbl_prebuilt/am62ax-sk/default_sbl_emmc_hs.cfg
    
  • Make sure IPC rpmsg echo application is built before running the flash script. (see IPC RP Message Echo)
  • To flash to the EVM, refer to Flash an example application . Only when giving the flash config file, point to the default_sbl_emmc_hs.cfg shown above.
  • Example, assuming SDK is installed at C:/ti/mcu_plus_sdk and this example and IPC application is built using makefiles, and Appimage is already created, in Windows,
      cd C:/ti/mcu_plus_sdk/tools/boot
      python uart_uniflash.py -p COM13 --cfg=C:/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62ax-sk/default_sbl_emmc_hs.cfg
    
  • If Linux PC is used, assuming SDK is installed at `~PSDK_LINUX_HS_IMAGE_PATH~/ti/mcu_plus_sdk/tools/boot/sbl_prebuilt/am62ax-sk//default_sbl_emmc_hs.cfg
  • Boot the EVM in eMMC boot mode to boot RTOS/Baremetal application on R5, M4 and A53 cores.

See Also

BOOTLOADER

Sample Output

After flashing and booting the EVM, you will see below output on the UART console (Complete log is not shown)

DMSC Firmware Version 9.1.8--v09.01.08 (Kool Koala)
DMSC Firmware revision 0x9
DMSC ABI revision 3.1

[BOOTLOADER_PROFILE] Boot Media       : eMMC
[BOOTLOADER_PROFILE] Boot Media Clock : 200.000 MHz
[BOOTLOADER_PROFILE] Boot Image Size  : 148 KB
[BOOTLOADER_PROFILE] Cores present    :
mcu-r5f0-0
r5f0-0
[BOOTLOADER PROFILE] System_init                      :      37940us
[BOOTLOADER PROFILE] Board_init                       :          0us
[BOOTLOADER PROFILE] Drivers_open                     :      60669us
[BOOTLOADER PROFILE] Board_driversOpen                :          0us
[BOOTLOADER PROFILE] Sciclient Get Version            :       9898us
[BOOTLOADER PROFILE] App_loadImages                   :       5806us
[BOOTLOADER PROFILE] App_loadSelfcoreImage            :       7259us
[BOOTLOADER_PROFILE] SBL Total Time Taken             :     121574us

Image loading done, switching to application ...
Starting MCU-r5f and 2nd stage bootloader

DMSC Firmware Version 9.1.8--v09.01.08 (Kool Koala)
DMSC Firmware revision 0x9
DMSC ABI revision 3.1

[BOOTLOADER_PROFILE] Boot Media       : eMMC
[BOOTLOADER_PROFILE] Boot Media Clock : 200.000 MHz
[BOOTLOADER_PROFILE] Boot Image Size  : 311 KB
[BOOTLOADER_PROFILE] Cores present    :
hsm-m4f0-0
r5f0-0
a530-0
c75ss0
[BOOTLOADER PROFILE] System_init                      :       1673us
[BOOTLOADER PROFILE] Board_init                       :          0us
[BOOTLOADER PROFILE] Drivers_open                     :      19520us
[BOOTLOADER PROFILE] Board_driversOpen                :          0us
[BOOTLOADER PROFILE] Sciclient Get Version            :       9990us
[BOOTLOADER PROFILE] App_loadImages                   :       5127us
[BOOTLOADER PROFILE] App_loadSelfcoreImage            :       7501us
[BOOTLOADER PROFILE] App_loadA53Images                :       6393us
[BOOTLOADER PROFILE] App_loadDSPImages                :       6850us
[BOOTLOADER_PROFILE] SBL Total Time Taken             :      57060us

Image loading done, switching to application ...
Starting RTOS/Baremetal applications
Hello World!