AM62Ax MCU+ SDK  09.02.00
DDR ECC Test MAIN ESM

Introduction

This example simulates a 1b and 2b ECC error for DDR and waits for interrupt via the MAIN ESM instance. On receiving the interrupt, the handler clears the ECC error bit and restore the original value. If the interrupt is not received the test fails.

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 freertos
Toolchain ti-arm-clang
Board am62ax-sk
Example folder examples/drivers/ddr/ddr_ecc_test_main_esm/

Steps to Run the Example

Note
DDR inline ECC can be configured in the sysconfig of other SBLs as well. If you are configuring ECC for different address region, change the DDR_ECC_REGION0_START macro in the example file for testing.

See Also

DDR

Sample Output

Shown below is a sample output when the application is run,

Waiting on Single bit Error Correction Interrupt...
1b ECC error detected
Waiting on Dual bit error detection Interrupt...
2b ECC error detected
All tests have passed!!