AM62Ax MCU+ SDK  11.01.00
Release Notes 11.01.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM62Ax MCU R5F, DM R5F, C75 SK-AM62A-LP EVM (referred to as am62ax-sk in code) Windows 10 64b or Ubuntu 22.04 64b

Features Added in This Release

Feature Module
ECC Functional Test example for single bit errors is added SDL
Updated DDR configuration from DDR configuration tool v10.30 DDR

Unsupported Features

Attention
TI would not support these feature on public e2e.
Feature Module
A53 FreeRTOS SMP support and A53 FreeRTOS SMP examples DPL, FreeRTOS

Dependent Tools and Compiler Information

Attention
It is recommended to use the TIFS version provided with the release for ensuring compatibility between TIFS and device manager. Using the TIFS from different MCU+SDK release is not recomended and may cause TIFS/ DM functionality to break.
Tools Supported CPUs Version
Code Composer Studio MCU-R5F, C75 20.2.0
SysConfig MCU-R5F, DM-R5F, C75 1.24.0, build 4150
TI ARM CLANG MCU-R5F, DM-R5F 4.0.1.LTS
GCC AARCH64 A53 9.2-2019.12
C7000-CGT C75 5.0.0.LTS
FreeRTOS Kernel MCU-R5F, DM-R5F, C75 11.1.0

SDK Components

SYSFW / TIFS

Version 11.01.05
Release Notes LINK
User Guide LINK

Key Features

OS Kernel

OS Supported CPUs SysConfig Support
FreeRTOS Kernel MCU-R5F, DM-R5F, C75 NA
FreeRTOS POSIX MCU-R5F NA
No RTOS MCU-R5F, DM-R5F NA

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support
Address Translate MCU-R5F, DM-R5F Yes FreeRTOS, NORTOS
Cache MCU-R5F, DM-R5F, C75 Yes FreeRTOS, NORTOS
Clock MCU-R5F, DM-R5F, C75 Yes FreeRTOS, NORTOS
CycleCounter MCU-R5F, DM-R5F, C75 NA FreeRTOS, NORTOS
Debug MCU-R5F, DM-R5F, C75 Yes FreeRTOS, NORTOS
Heap MCU-R5F, DM-R5F, C75 NA FreeRTOS, NORTOS
Hwi MCU-R5F, DM-R5F, C75 Yes FreeRTOS, NORTOS
MPU MCU-R5F, DM-R5F, C75 Yes FreeRTOS, NORTOS
Semaphore MCU-R5F, DM-R5F, C75 NA FreeRTOS, NORTOS
Task MCU-R5F, DM-R5F, C75 NA FreeRTOS
Timer MCU-R5F, DM-R5F Yes FreeRTOS, NORTOS

Secondary Bootloader (SBL)

SBL Mode Supported CPUs SysConfig Support PHY Support DMA Support OS support
OSPI NAND DM-R5F Yes No Yes NORTOS
EMMC DM-R5F Yes NA NA NORTOS
UART DM-R5F Yes NA No NORTOS

SOC Device Drivers

Note
See the updated MCASP usage guidelines in MCASP for changes in MCASP driver
Peripheral Domain Supported CPUs SysConfig Support
DDR Main DM-R5F Yes
ECAP Main DM-R5F , C75 Yes
EPWM Main MCU-R5F, DM-R5F , C75 Yes
EQEP Main DM-R5F , C75 Yes
GPIO MCU MCU-R5F, DM-R5F , C75 Yes
Main MCU-R5F, DM-R5F , C75 Yes
I2C Main MCU-R5F, DM-R5F , C75 Yes
MCU MCU-R5F, DM-R5F Yes
Wakeup MCU-R5F, DM-R5F Yes
IPC Main MCU-R5F, DM-R5F , C75 Yes
MCAN MCU MCU-R5F Yes
MCASP Main DM-R5F , C75 Yes
MCSPI Main MCU-R5F, DM-R5F Yes
MCU MCU-R5F, DM-R5F Yes
MMCSD Main DM-R5F Yes
OSPI Main DM-R5F Yes
Pinmux Main MCU-R5F, DM-R5F , C75 Yes
MCU MCU-R5F, DM-R5F , C75 Yes
Wakeup MCU-R5F, DM-R5F , C75 Yes
RTC Main MCU-R5F, DM-R5F Yes
SOC NA MCU-R5F, DM-R5F , C75 Yes
SCIClient NA MCU-R5F, DM-R5F , C75 Yes
UART Main MCU-R5F, DM-R5F , C75 Yes
MCU MCU-R5F, DM-R5F Yes
Wakeup DM-R5F Yes
UDMA Main MCU-R5F, DM-R5F , C75 Yes
Note
Refer Accessing main and wakeup domain peripherals from MCU domain for accessing main/wakeup peripherals from MCU Domain.

Board Device Drivers

Peripheral Supported CPUs SysConfig Support
EEPROM MCU-R5F Yes
Flash DM-R5F Yes
LED MCU-R5F Yes

SDL

SDL Module Supported CPUs SysConfig Support
MCRC MCU-R5F No
ESM MCU-R5F No
VTM MCU-R5F No
DCC MCU-R5F No
RTI MCU-R5F No
POK MCU-R5F No
STOG MCU-R5F No
MTOG MCU-R5F No
ECC MCU-R5F No
PBIST MCU-R5F No
LBIST MCU-R5F No
ROM Checksum MCU-R5F No

Fixed Issues

ID Head Line Module Applicable Releases
EXT_EP-12721 ECC TCM example cannot be built for AM62A SDL 11.01.00
EXT_SITMPUSW-105 MMCSD driver uses snprintf function from libc MMCSD 11.01.00
EXT_SITMPUSW-77 Modify Read capture delay logic for Tap Mode OSPI 11.00.00
EXT_SITMPUSW-106 OSPI Phy Tuning Data is not written correctly in Flash_norOspiOpen() OSPI 10.01.00

Known Issues

ID Head Line Module Reported in release Workaround
EXT_SITMPUSW-1085 Flash_eraseSector and Flash_norOspiEraseSector does not erases the mentioned sector. Flash 11.00.00 No known workaround
EXT_SITMPUSW-28 Outstanding mailbox messages prevent suspend IPC 08.03.00 No known workaround
EXT_SITMPUSW-107 AM62A : Reset Isolation sequence is wrong Reset 11.00.00 No known workaround
EXT_SITMPUSW-109 Wrong comments on HwiP_inISR() API DPL 11.00.00 No known workaround
EXT_SITMPUSW-78 MMCSD Sysconfig provides options to configure PHY type MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-84 MMCSD error recovery sequence isn't implemented correctly MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-110 eMMC Init Code Missing DLL Register Settings needed for Initial Legacy SDR Mode Phase MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-113 eMMC PHY I/O Calibration not getting executed during eMMC boot MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-114 MMCSD_enableBootPartition implements two mutually exclusive concepts as one function MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-123 MMCSD driver does not follow the SWITCH command sequence correctly MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-124 EXTCSD HS_TIMING register is set incorrectly at certain places in the driver MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-125 MMCSD driver uses infinite loop instead of timeout for checking fields of PRESENTSTATE register MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-126 Timing issues with MMCSD host controller driver MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-128 EMMC timiing parameters to be changed based on SOC and MMC instance MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-117 Linux Kernel IPC Examples are broken IPC 11.00.00 Change ti.ipc4.ping-pong to rpmsg-client-sample in the example
EXT_SITMPUSW-120 C7x task size/alignment should be 8KB (not 16KB) FreeRTOS 11.00.00 Change the stack alignment
EXT_SITMPUSW-121 FORCE bit not book keeped properly for MCSPI DMA mode of operation MCSPI 11.00.00 No known workaround
EXT_SITMPUSW-122 HSM core does not boot SBL 11.00.00 No known workaround
EXT_SITMPUSW-133 Falcon Boot through SBL is not supported SBL 09.02.00 No known workaround
EXT_SITMPUSW-136 dmautils_autoincrement example fails on AM62A SBL 09.02.00 No known workaround
EXT_EP-12281 AM62A: ECC: ECC is failing for 2 Bit VTM selftest - ECC Unit test fails at the API call ECC_Test_runECC2BitVTM0selfTest() SDL 10.01.00 No known workaround
EXT_EP-12276 ECC: Firewall related aggregators failures - ECC Aggregators SDL_SMS0_SMS_TIFS_ECC, SDL_SMS0_SMS_HSM_ECC and SDL_SA3_SS0_SA3SS_AM62A_DMSS_ECCAGGR fail because of firewall access issues faced by SDL SDL 10.01.00 No known workaround
EXT_EP-12280 Running MCU LBIST on SBL causes JTAG connection issues to MCU R5F - Running MCU LBIST on SBL causes JTAG connection issues to MCU R5F on AM62ax SDL 09.00.00 No known workaround
EXT_EP-12283 ECC aggregators CPSW0, CSI RX are failing on AM62A and CPSW0 on AM62D. SDL 09.00.00 No known workaround

Limitations

S.No Head Line Module
1 The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK NA
2 PHY mode not supported for OSPI NAND SBL on DDR mode. It is supported for SDR mode only Bootloader

Upgrade and Compatibility Information

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

The below table captures the list of migration document sections when migrating from one version to another. The migration for a partcluar module will be applicable, if you are migrating from older version listed to newer version listed on the table below.

Module Migration guide Older version Newer version
Bootloader Bootloader Migration Guidelines<= 10.01.00 >= 11.00.00

Networking

Module Affected API Change
TSN notify_linkchange notify_linkchange function is renamed to cb_lld_notify_linkchange, include path <tsn_combase/tilld/cb_lld_ethernet.h> in the file that uses cb_lld_notify_linkchange.