Introduction
The following shows an example of SDL MTOG API usage by the application to set up the TOG module with the usage of the various APIs. Events can be monitored by enabling the events in the associated ESM instance.
Use Cases
| Use Case | Description |
| UC-1 | WKUP0 INSTANCE |
| UC-2 | WKUP1 INSTANCE |
Supported Combinations
| Parameter | Value |
| CPU + OS | mcu-r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am62ax-sk |
| Example folder | examples/sdl/mtog/mtog_example/ |
Steps to Run the Example
See Also
MTOG
Sample Output
Shown below is a sample output when the application is run,
TIMER_ESM_init: Init MCU ESM complete
Starting MTOG test on MCU MTOG0, index 1...
MTOG Status Register Value for the instance1 = 2
MTOG Reset done
Delta MTOG prep time in micro secs 5
Delta MTOG execution time in micro secs 6740
Delta MTOG restore time in micro secs 1
MTOG complete for MCU MTOG0
Sdl mtog instance 1 passed
Starting MTOG test on MCU MTOG0, index 2...
MTOG Status Register Value for the instance2 = 1
MTOG Reset done
Delta MTOG prep time in micro secs 4
Delta MTOG execution time in micro secs 6442
Delta MTOG restore time in micro secs 0
MTOG complete for MCU MTOG0
Sdl mtog instance 2 passed
MTOG Saftey Example passed.