AM62Ax MCU+ SDK  10.00.00
TIFS_SAFETY_CHECKERS

TIFS Safety Checkers library APIs are integrated into the safety application to verify the firewall configuration and validate the FWL configuration against golden reference.

Features Supported

The module supports below API's for the application

  • API to request TIFS to open firewall.
  • API to generate Golden Reference using the list of firewall registers specified.
  • API compares the Golden Reference with runtime firewall register values and return success or failure.
  • API to request TIFS to close firewall.

SysConfig Features

  • None

Features NOT Supported

  • None

Important Usage Guidelines

Steps to update board configuration for TIFS Safety Checkers:

  • Add below lines to the file " ${mcu_plus_sdk}/source/drivers/sciclient/sciclient_default_boardcfg/{board}/sciclient_defaultBoardcfg_security.c"
/* SA2UL RM config */
.sa2ul_auth_cfg = {
.subhdr = {
.size = 0,
},
.auth_resource_owner = 0,
.enable_saul_psil_global_config_writes = 0x5A,
.safety_host_present = 0x5A,
.safety_host = host_id
},
Note
host_id = 0x1E for mcu-r5f
  • Use the following commands to build the Boardcfg changes For GP and HS-FS
    cd ${mcu_plus_sdk}/tools/sysfw/boardcfg/
    make SOC={board}
    cd ${mcu_plus_sdk}
    make scrub SOC={board}
    make all SOC={board}
    For HS-SE
    cd ${mcu_plus_sdk}/tools/sysfw/boardcfg/
    make SOC={board} DEVICE_TYPE=HS
    cd ${mcu_plus_sdk}
    make scrub SOC={board} DEVICE_TYPE=HS
    make all SOC={board} DEVICE_TYPE=HS

Example Usage

The following shows an example of TIFS Safety Checkers API usage

Include the below file to access the APIs

#include "../../src/safety_checkers_tifs.h"

Request the TIFS to open firewall

Uses the pointer to firewall configuration pFwlConfig as input and updates pFwlConfig with the register dump of the firewall registers specified.

SafetyCheckers_tifsGetFwlCfg(pFwlConfig, gSize);

Verify and save firewall configuration as Golden Reference

Compare the golden reference with runtime firewall register values and return success or failure.

while (i > 0)
{
status = SafetyCheckers_tifsVerifyFwlCfg(pFwlConfig, gSafetyCheckersTifsCfgSize);
if (status == SAFETY_CHECKERS_REG_DATA_MISMATCH)
{
SAFETY_CHECKERS_log("\n Firewall register mismatch with Golden Reference !!\r\n");
}
SafetyCheckersApp_softwareDelay();
i--;
}
if (status == SAFETY_CHECKERS_SOK)
{
SAFETY_CHECKERS_log("\n No firewall register mismatch with Golden Reference \r\n");
}

Request the TIFS to close firewall

API

TIFS Safety Checkers Library

TISCI_BOARDCFG_SA2UL_CFG_MAGIC_NUM_RSVD
#define TISCI_BOARDCFG_SA2UL_CFG_MAGIC_NUM_RSVD
Definition: tisci_boardcfg_macros.h:91
SafetyCheckers_tifsGetFwlCfg
int32_t SafetyCheckers_tifsGetFwlCfg(SafetyCheckers_TifsFwlConfig *fwlConfig, uint32_t size)
API uses the pointer to firewall configuration fwlConfig as input and updates fwlConfig with the regi...
status
uint32_t status
Definition: tisci_lpm.h:1
SafetyCheckers_tifsVerifyFwlCfg
int32_t SafetyCheckers_tifsVerifyFwlCfg(const SafetyCheckers_TifsFwlConfig *fwlConfig, uint32_t size)
API compares the fwlConfig (golden reference) with runtime firewall register values and return succes...
SafetyCheckers_tifsReqFwlOpen
int32_t SafetyCheckers_tifsReqFwlOpen(void)
API to request TIFS to open firewall.
SafetyCheckers_tifsReqFwlClose
int32_t SafetyCheckers_tifsReqFwlClose(void)
API to request TIFS to close firewall.
host_id
uint8_t host_id
Definition: tisci_boardcfg.h:0