AM62Ax MCU+ SDK  10.00.00
SA3UL Random Number Generator Test

Introduction

This example demonstrates the Random number generation using SA3UL module.

Supported Combinations

Parameter Value
CPU + OS a53ss0-0 nortos
Toolchain arm.gnu.aarch64-none
Board am62ax-sk
Example folder examples/security/crypto/sa3ul_rng/sa3ul_rng.c

Steps to Run the Example

See Also

SA3UL

Sample Output

Shown below is a sample output when the application is run.

CCS Console:

All tests have passed!!
[SA3UL] Sa3ul Rng example started ...
[SA3UL] Sa3ul Rng output word 1 -- 0x3704DD0A
[SA3UL] Sa3ul Rng output word 2 -- 0x68719DEA
[SA3UL] Sa3ul Rng output word 3 -- 0x3A2733EE
[SA3UL] Sa3ul Rng output word 4 -- 0x943F007E
[SA3UL] Sa3ul Rng output word 1 -- 0xCE83C20D
[SA3UL] Sa3ul Rng output word 2 -- 0xAEB445B0
[SA3UL] Sa3ul Rng output word 3 -- 0xE052FEC9
[SA3UL] Sa3ul Rng output word 4 -- 0x713231C3
[SA3UL] Sa3ul Rng output word 1 -- 0xD5CF553B
[SA3UL] Sa3ul Rng output word 2 -- 0x1AB11E5F
[SA3UL] Sa3ul Rng output word 3 -- 0x25163494
[SA3UL] Sa3ul Rng output word 4 -- 0x5CD0432F
[SA3UL] Sa3ul Rng output word 1 -- 0x8372B743
[SA3UL] Sa3ul Rng output word 2 -- 0x75AA97AC
[SA3UL] Sa3ul Rng output word 3 -- 0x59F277C7
[SA3UL] Sa3ul Rng output word 4 -- 0x8DFC768C
[SA3UL] Sa3ul Rng output word 1 -- 0xAF3B154C
[SA3UL] Sa3ul Rng output word 2 -- 0x3A93F540
[SA3UL] Sa3ul Rng output word 3 -- 0xC3174A84
[SA3UL] Sa3ul Rng output word 4 -- 0xA361D316
[SA3UL] Sa3ul Rng example completed!!
All tests have passed!!