RM Safety Checker (SAFETY_CHECKERS-RM) provided APIs which are integrated into the safety application to verify the RM modules configuration and validate the runtime RM moudules configuration against golden reference.
SAFETY_CHECKERS-RM library includes the following implementation:
This example demonstrates how to use SAFETY_CHECKERS-RM library APIs.
In generation of RM modules config, Safety application shall call the RM read APIs to access the configuration registers from the Safety Checkers library running in the Safety Core. Safety checkers returns RM modules config to the safety application. Safety application validates the RM modules configuration and save it as a golden reference in a non-volatile memory. This initializes the Safety Application and gathers the initial configuration data.
In validate RM module config stage, Safety application provides golden reference to the RM safety checker and Safety checker will validates at defined intervals. RM safety checker reads the RM modules registers at runtime and validate they are matching with the golden state for modules in safety loop. Safety checker will return success or failure after validates against the golden reference.
Parameter | Value |
---|---|
CPU + OS | mcu-r5fss0-0 freertos |
r5fss0-0 freertos | |
Toolchain | ti-arm-clang** |
arm.gnu.aarch64-none | |
Boards | am62ax-sk |
Example folder | source/safety_checkers/examples/ |
Shown below is a sample output when the application is run,