This example just does driver and board initialization and prints the string, Hello World! on UART console.
Parameter | Value |
---|---|
CPU + OS | mcu-r5fss0-0 nortos |
mcu-r5fss0-0 freertos | |
a53ss0-0 nortos | |
a53ss0-0 freertos | |
a53ss0-0 freertos-smp | |
c75ss0-0 freertos | |
Toolchain | ti-arm-clang |
arm.gnu.aarch64-none | |
Boards | am62ax-sk |
Example folder | examples/hello_world/ |
Shown below is a sample output when the application is run,