This example demonstrates the UART RX and TX operation in callback, interrupt mode of operation. This example receives 8 characters and echos back the same. The application ends when the user types 8 characters.
Parameter | Value |
---|---|
CPU + OS | mcu-r5fss0-0 nortos |
| a53ss0-0 nortos Toolchain | ti-arm-clang | arm.gnu.aarch64-none Board | am62ax-sk Example folder | examples/drivers/uart/uart_echo_callback
Shown below is a sample output when the application is run, Please note that application prints in both CCS and UART console. In UART console you need to type 8 characters.
CCS Console:
UART Console: