Introduction
This example shows usage of RP Message APIs to each multi-byte messages between different CPUs
In this example,
- One "main" CPU, sends multi-byte messages to other "remote" CPUs using the RP Message APIs
- The "remote" CPUs, then echo back the same message to the main CPUs
- Once all messages are echoed the main CPU exits. The remote CPUs remain waiting to receive new messages.
Supported Combinations
Parameter | Value |
CPU + OS | mcu-r5fss0-0 nortos |
r5fss0-0 freertos |
a53ss0-0 nortos |
a53ss0-0 freertos-smp |
c75ss0-0 freertos |
Toolchain | ti-arm-clang |
arm.gnu.aarch64-none |
Boards | am62ax-sk |
Example folder | examples/drivers/ipc/ipc_rpmsg_echo |
Note
There are two examples for A53 cores, a53ss0-0_freertos-smp and a53ss0-0_nortos. For single core application use a53ss0-0_nortos and for smp application use a53ss0-0_freertos-smp
Steps to Run the Example
- Note
- This is a
system
or multi-core project, so refer to system project build instructions for CCS project or makefiles when building the example.
- When using CCS projects to build, import the system CCS project and build it using the CCS project menu (see Using SDK with CCS Projects). This will build all the dependant CPU projects as well
- When using makefiles to build, build the system makefile using make command (see Using SDK with Makefiles). This will build all the dependant CPU makefiles as well.
- Launch a CCS debug session and run the executables, see CCS Launch, Load and Run
- Attention
- As the wake-up R5 is the device manager, it needs to be started by the SBL. So it can not be loaded through CCS. It should be flashed and booted through SBL.
- Refer Flash an example application for flashing the application.
- This is a multi-core example. Hence the executables should be loaded and run for all the above mentioned cores
- The application has a sync mechanism at the start which waits for all cores to start before doing the test. Hence the cores can be loaded and run in any sequence.
See Also
IPC RPMessage
Sample Output
Shown below is a sample output when the application is run,
[mcu-r5f0-0] 32.119999s : [IPC RPMSG ECHO] Remote Core waiting for messages from main core ... !!!
[a530-0] 66.509049s : [IPC RPMSG ECHO] Remote Core waiting for messages from main core ... !!!
[c75ss0] 0.000999s : [IPC RPMSG ECHO] Remote Core waiting for messages from main core ... !!!
[IPC RPMSG ECHO] Message exchange started by main core !!!
[IPC RPMSG ECHO] All echoed messages received by main core from 3 remote cores !!!
[IPC RPMSG ECHO] Messages sent to each core = 10
[IPC RPMSG ECHO] Number of remote cores = 3
[IPC RPMSG ECHO] Total execution time = 1779 usecs
[IPC RPMSG ECHO] One way message latency = 29650 nsec
All tests have passed!!
[mcu-r5f0-0] 32.622999s : [IPC RPMSG ECHO] Received and echoed 10 messages ... !!!
[mcu-r5f0-0] 32.622999s : All tests have passed!!
[a530-0] 67.013217s : [IPC RPMSG ECHO] Received and echoed 10 messages ... !!!
[a530-0] 67.013221s : All tests have passed!!
[c75ss0] 0.504999s : [IPC RPMSG ECHO] Received and echoed 10 messages ... !!!
[c75ss0] 0.505999s : All tests have passed!!