- Attention
- Please note that this driver is supported only on DM R5(WKUP R5) as part SBL examples. It is not supported on MCU-R5.
The Octal Serial Peripheral Interface (OSPI) module is a kind of Serial Peripheral Interface (SPI) module which allows single, dual, quad or octal read and write access to external flash devices. The OSPI module is used to transfer data, either in a memory mapped direct mode (for example a processor wishing to execute code directly from external flash memory), or in an indirect mode where the module is set-up to silently perform some requested operation, signaling its completion via interrupts or status registers.
Features Supported
- Support for single, dual, quad (QSPI mode) or octal I/O instructions.
- Supports dual Quad-SPI mode for fast boot applications.
- Memory mapped ‘direct’ mode of operation for performing flash data transfers and executing code from flash memory.
- Programmable delays between transactions.
- Legacy mode allowing software direct access to low level transmit and receive FIFOs, bypassing the higher layer processes.
- An independent reference clock to decouple bus clock from SPI clock – allows slow system clocks.
- Programmable baud rate generator to generate OSPI clocks.
- Supports BOOT mode.
- Handling ECC errors for flash devices with embedded correction engine.
SysConfig Features
- Note
- It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
- OSPI instance name
- Input clock frequency to be used for OSPI module
- Input clock divider which decides the baud-rate at which the flash will be read
- Chip Select
- In advanced config, you can choose various parameters like frame format, decoder chip select, read dummy cycles etc.
- Pinmux configurations for the OSPI instance
OSPI Phy Tuning Algorithm
The OSPI tuning algorithm works as follows:
- Step 1 Find Golden Primary RxLow
To find the RxDLL boundaries, we fix a valid TxDLL and search through RxDLL range, rdDelay values.
As we are not sure of a valid TxDLL we use a window of TxDLL values to find the RxDLL boundaries. Rx_DLL
▲
│ ++++++++++++++++
127 │ ++++++++++++++
│ x ++++++++++++
│ xx +++++++++++
│ xxx ++++++++++
│ xxxx +++++++++
│ xxxxx ++++++++
│ │ xxx│xx +++++++
│ │ xxx│xxx ++++++
│ │ xxx│xxxx +++++
│ │ xxx│xxxxx ++++
│ │ xxx│xxxxxx +++
Search │ │ xxx│xxxxxxx ++
Rx_Low ──┼─┤►xxx│xxxxxxxx +
│ │ │
─┼─┼────┼------────► Tx_DLL
0│ │ │ 127
│ │
│ │
Tx_Low Tx_Low
Start End
- Step 2 Find Golden Secondary RxLow
Search for one more rxLow at different txDl, To find Secondary rxHigh we use the txDLL + Search_offset value of rxLow.
- Step 3 Select minimum of primary rxLow and secondary rxLow Value
- Pick minimum value of rxDLL between rxLow and sec_rxLow.
- Pick Minimum value of rdDelay(read_delay) between rxLow and sec_rxLow.
Primary
Search | Secondary
Search | Final Point |
Fail | Fail | Return Fail |
Fail | Pass | Return Fail |
Pass | Fail | Return Fail |
Pass | Pass | RxDll = Min(Primary, Secondary)
RdDelay = Min(Primary, Secondary)
TxDll = Primary |
- Step 4 Find Golden Primary Rx High
To find rxHigh we use the txDLL values of rxLow.
Start the rdDelay (Read delay) from maximum and decrement it.
As these are valid values and rxHigh rdDelay is always >= rxLow rdDelay. Rx_DLL
▲
127 │ ▲+++++++++++++++
Search │ │ ++++++++++++++
Rx_High────┼──►│ ++++++++++++
on Fixed │ │x +++++++++++
Tx_DLL │ │xx ++++++++++
│ │xxx +++++++++
│ │xxxx ++++++++
│ ▼xxxxx +++++++
│ Xxxxxxx ++++++
│ Xxxxxxxx +++++
│ Xxxxxxxxx ++++
│ Xxxxxxxxxx +++
│ Xxxxxxxxxxx ++
│ Xxxxxxxxxxxx +
│
─┼------------───► Tx_DLL
0│ 127
- Step 5 Find Golden Secondary Rx High
To find Secondary rxHigh we use the txDLL + Search_offset value of rxLow.
Start the rdDelay (Read delay) from maximum and decrement it.
As these are valid values and rxHigh rdDelay is always >= rxLow rdDelay.
- Step 6 Select maximum of primary and secondary rxHigh value
- Compare the Primary and Secondary point.
- Pick the point which has passing maximum rxDll.
Primary
Search | Secondary
Search | Final Point |
Fail | Fail | Return Fail |
Fail | Pass | Return Fail |
Pass | Fail | Return Fail |
Pass | Pass | If(secondary.rxDll > primary.rxDll)
Pick Secondary search point
Else
Pick Primary search point |
- Step 7 Do a backup Search in case rxLow and rx High has same read delay values
Check a different point if the rxLow and rxHigh are on the same rdDelay.
This avoids mistaking the metastability gap for an rxDLL boundary.
- Find backup rx Low Find the rxDLL boundaries using the TxDLL window at the higher end .
We start the window_end and decrement the TxDLL value until we find the valid point. Rx_DLL
▲
│ ++++++++++++++++
127 │ ++++++++++++++++
│ ++++++++++++++++
│ +++++++++++++++
│ +++++++++│++++│
│ ++++++++│++++│
│ x +++++++│++++│
│ xx ++++++│++++│
│ xxx +++++│++++│
│ xxxx ++++│++++│
│ xxxxx +++│++++│
│ xxxxxx ++│++++│
│ xxxxxxx +│++++│ Search
│ xxxxxxxx │++++◄─────── Rx_Low
│ │ │
─┼──────────────┼────┤► Tx_DLL
0│ │ │ 127
│ │
Tx_High Tx_High
Start End
- Find backup sec rxLow
Search for one more rxLow at different txDll, we use the txDLL - Search_offset value of rxLow.
- Select minimum of backup rxLow and backup sec rxLow
- Pick minimum value of rxDLL between rxLow and sec_rxLow.
- Pick Minimum value of rdDelay(read_delay) between rxLow and sec_rxLow.
- Find backup primary rxHigh search Find rxDLL Max
Start the rdDelay (Read delay) from maximum and decrement it.
Rx_DLL
127 ▲
│ +++++++++++++++▲ Search Rx_High
│ +++++++++++++++│◄──────────── on Fixed Tx_DLL
│ +++++++++++++++│
│ ++++++++++++++│
│ +++++++++++++│
│ ++++++++++++│
│ x +++++++++++▼
│ xx +++++++++++
│ xxx ++++++++++
│ xxxx +++++++++
│ xxxxx ++++++++
│ xxxxxx +++++++
│ xxxxxxx ++++++
│ xxxxxxxx ++++
│
─┼────────────────────► Tx_DLL
0│ 127
- Find backup secondary rxHigh search
Search for one more rxHigh at different txDll, we use the txDLL - Search_offset value of rxLow.
- Select maximum of backup primary and secondary rxhigh
Compare the Primary and Secondary point.
Pick the point which has passing maximum rxDll.
Primary
Search | Secondary
Search | Final Point |
Fail | Fail | Return Fail |
Fail | Pass | Return Fail |
Pass | Fail | Return Fail |
Pass | Pass | If(secondary.rxDll > primary.rxDll)
Pick Secondary search point
Else
Pick Primary search point |
- Step 8 Find golden TxLow Look for txDLL boundaries at 1/4 of rxDLL window.
Find txDLL Min.
Rx_DLL
127 ▲
│ ++++++++++++++++
Rx_High │ ++++++++++++++
───────┼──►x ++++++++++++
│ xx +++++++++++
│ xxx ++++++++++
│ xxxx +++++++++
Fix Rx_DLL │ xxxxx ++++++++
1/4 between │ xxxxxx +++++++
Rx_High and │ xxxxxxx ++++++
Rx_Low │ xxxxxxxx +++++
──────┼─► ◄───┬──► ++++
│ xxxx│xxxxx +++
Rx_Low │ xxxx│xxxxxx ++
──────┼──►xxxx│xxxxxxx +
│ │
─┼───────┼───────────► Tx_DLL
0│ │ 127
│
Search Tx_Low
- Step 9 Find golden TxHigh
Find txDLL Max.
Start the rdDelay (Read delay) from maximum and decrement it.
Rx_DLL
127 ▲
│ +++++++++++++++++
Rx_High │ +++++++++++++++
───────┼──►x +++++++++++++
│ xx ++++++++++++
│ xxx +++++++++++
│ xxxx ++++++++++
Fix Rx_DLL │ xxxxx +++++++++
1/4 between │ xxxxxx ++++++++
Rx_High and │ xxxxxxx +++++++
Rx_Low │ xxxxxxxx ++++++
──────┼─► xxxxxxxxx ◄─┬─►
│ xxxxxxxxxx +│++
Rx_Low │ xxxxxxxxxxx │++
──────┼──►xxxxxxxxxxxx │++
│ │
─┼─────────────────┼─► Tx_DLL
0│ │127
Search Tx_Max
- Step 10 Do a backup Search in case rxLow and rx High has same read delay values
Check a different point if the txLow and txHigh are on the same rdDelay.
This avoids mistaking the metastability gap for a txDLL boundary.
- Find a backup primary txLow
Look for txDLL boundaries at 3/4 of rxDLL window.
Find txDLL Min.
Rx_DLL
127 ▲
│
Rx_High──┼──►+++++++++++++++++
Fix Rx_DLL │ +++++++++++++++++
3/4 of │ +++++++++++++++++
Rx_High ─┼─► ◄───┬───►++++++++
and Rx_Low │ ++│++++++++++++
│ +│++++++++++++
│ x │++++++++++++
│ xx │++++++++++++
│ xxx │ +++++++++++
│ xxxx│ ++++++++++
│ xxxx│ +++++++++
│ xxxx│x ++++++++
│ xxxx│xx +++++++
Rx_Low──┼──►xxxx│xxx ++++++
│ │
─┼───────┼────────────► Tx_DLL
0│ │ 127
Search Tx_Min
- Find a backup primary txHigh
Find txDLL Max.
Start the rdDelay (Read delay) from maximum and decrement it.
Rx_DLL
127
▲
│
Rx_High──┼──►+++++++++++++++++
│ +++++++++++++++++
Fix Rx_DLL │ +++++++++++++++++
3/4 of ────┼─► +++++++◄────┬───►
Rx_High │ ++++++++++│++++
and │ +++++++++│++++
Rx_Low │ x ++++++++│++++
│ xx +++++++│++++
│ xxx ++++++│++++
│ xxxx +++++│++++
│ xxxxx ++++│++++
│ xxxxxx +++│++++
│ xxxxxxx ++│++++
Rx_Low──┼──►xxxxxxxx +│++++
│ │
─┼───────────────┼────► Tx_DLL
0│ │ 127
Search Tx_Max
- Step 11 Find bottom left and top right corners
These are theoretical corners. They may not actually be "good" points.
But the longest diagonal of the shmoo will be between these corners.
- Step 12 Find the tuning point
- Step1 Find the equation of diagonal between topRight(rxHigh,txHigh) and bottomLeft(rxLow,txLow) points.
- Step2 Find gapLow, last point along the slope of bottom left read delay region.
- Step3 If top right and bottom left have same read delay, put tuning point in the middle and adjust for temperature.
- Step4 If top right and bottom left have different read delays, find gapHigh, the starting point along the slope of top left read delay region.
- Step5 Find len1 = gapLow - topLeft, len2 = topRight - gapHigh.
- Step6 Choose the read Delay region with maximum length.
- Step7 Place the Phy tuning point in the corner farthest from the gap.
Features not Supported
- PHY mode is not supported yet.
- XIP mode is not supported yet.
Example Usage
Include the below file to access the APIs
Instance Open Example
Instance Close Example
API
APIs for OSPI