|
AM62Ax MCU+ SDK
09.01.00
|
|
Go to the documentation of this file.
34 #ifndef SDL_SOC_RTI_H_
35 #define SDL_SOC_RTI_H_
37 #include <sdl/include/am62ax/sdlr_soc_baseaddress.h>
48 #define SDL_RTI_MAX_INSTANCE (0x07U)
49 #define INSTANCE_INVALID (0x0U)
84 SDL_RTI1_CFG_BASE, SDL_RTI2_CFG_BASE, SDL_RTI3_CFG_BASE, \
85 SDL_RTI4_CFG_BASE, SDL_WKUP_RTI0_CFG_BASE, \
@ SDL_INSTANCE_RTI2_CFG
Definition: sdl_soc_rti.h:70
@ SDL_INSTANCE_MCU_RTI0_CFG
Definition: sdl_soc_rti.h:67
@ SDL_INSTANCE_INVALID
Definition: sdl_soc_rti.h:74
@ SDL_INSTANCE_RTI3_CFG
Definition: sdl_soc_rti.h:71
@ SDL_INSTANCE_RTI4_CFG
Definition: sdl_soc_rti.h:72
#define SDL_RTI_MAX_INSTANCE
Definition: sdl_soc_rti.h:48
@ SDL_INSTANCE_RTI0_CFG
Definition: sdl_soc_rti.h:68
@ SDL_INSTANCE_RTI1_CFG
Definition: sdl_soc_rti.h:69
static uint32_t SDL_RTI_baseAddress[SDL_RTI_MAX_INSTANCE+1U]
Definition: sdl_soc_rti.h:83
@ SDL_INSTANCE_WKUP_RTI0
Definition: sdl_soc_rti.h:73
SDL_RTI_InstanceType
Definition: sdl_soc_rti.h:65
int32_t SDL_RTI_getBaseaddr(SDL_RTI_InstanceType instance, uint32_t *baseAddr)