SOC | Supported CPUs | EVM | Host PC |
---|---|---|---|
AM62Ax | MCU R5F, DM R5F, A53, C75 | SK-AM62A-LP EVM (referred to as am62ax-sk in code) | Windows 10 64b or Ubuntu 22.04 64b |
Feature | Module |
---|---|
FreeRTOS and FreeRTOS-SMP dual core support on A53 | OS |
FreeRTOS support on C75 | OS |
SBL support for booting C75 Core | SBL |
SBL OSPI NAND, SBL EMMC, SBL UART and SBL SD support booting RTOS/baremetal on A53 Core | SBL |
SBL OSPI NAND runs MCU LBIST and PBIST before loading MCU R5F | SBL |
Boottime optimization: Use Authentication type 2 | SBL |
DDR inline ECC | DDR |
GPIO, I2C, IPC, Sciclient, UDMA and UART driver support on A53 | Drivers |
I2C, IPC, Sciclient and UART driver support on C75 | Drivers |
EMMC init time optimized | EMMC |
EMMC HS200 support | EMMC |
McASP support on C75 and DM-R5F | MCASP |
MCU reset isolation | Safety |
Example for monitoring firewall exceptions | Security |
Feature | Module |
---|---|
A53 FreeRTOS SMP support and A53 FreeRTOS SMP examples | DPL, FreeRTOS |
Tools | Supported CPUs | Version |
---|---|---|
Code Composer Studio | MCU-R5F, C75, A53 | 12.5.0 |
SysConfig | MCU-R5F, DM-R5F, C75, A53 | 1.18.0, build 3266 |
TI ARM CLANG | MCU-R5F, DM-R5F | 3.2.0.LTS |
GCC AARCH64 | A53 | 9.2-2019.12 |
C7000-CGT | C75 | 3.1.0LTS |
FreeRTOS Kernel | MCU-R5F, DM-R5F, C75, A53 | 10.4.3 |
OS | Supported CPUs | SysConfig Support |
---|---|---|
FreeRTOS Kernel | MCU-R5F, DM-R5F, A53, C75 | NA |
FreeRTOS POSIX | MCU-R5F, A53 | NA |
FreeRTOS SMP | A53(Dual Core) | NA |
NO RTOS | MCU-R5F, DM-R5F, A53 | NA |
Module | Supported CPUs | SysConfig Support | OS support |
---|---|---|---|
Address Translate | MCU-R5F, DM-R5F | YES | FreeRTOS, NORTOS |
Cache | MCU-R5F, DM-R5F, A53, C75 | YES | FreeRTOS, NORTOS |
Clock | MCU-R5F, DM-R5F, A53, C75 | YES | FreeRTOS, NORTOS |
CycleCounter | MCU-R5F, DM-R5F, A53, C75 | NA | FreeRTOS, NORTOS |
Debug | MCU-R5F, DM-R5F, A53, C75 | YES | FreeRTOS, NORTOS |
Heap | MCU-R5F, DM-R5F, A53, C75 | NA | FreeRTOS, NORTOS |
Hwi | MCU-R5F, DM-R5F, A53, C75 | YES | FreeRTOS, NORTOS |
MPU | MCU-R5F, DM-R5F, A53, C75 | YES | FreeRTOS, NORTOS |
Semaphore | MCU-R5F, DM-R5F, A53, C75 | NA | FreeRTOS, NORTOS |
Task | MCU-R5F, DM-R5F, A53, C75 | NA | FreeRTOS |
Timer | MCU-R5F, DM-R5F, A53 | YES | FreeRTOS, NORTOS |
SBL Mode | Supported CPUs | SysConfig Support | PHY Support | DMA Support | OS support |
---|---|---|---|---|---|
OSPI NAND | DM-R5F | YES | No | Yes | NORTOS |
EMMC | DM-R5F | YES | NA | NA | NORTOS |
UART | DM-R5F | YES | NA | No | NORTOS |
Peripheral | Domain | Supported CPUs | SysConfig Support |
---|---|---|---|
DDR | Main | DM-R5F | YES |
GPIO | MCU | MCU-R5F, DM-R5F | YES |
Main | MCU-R5F, DM-R5F | YES | |
I2C | Main | MCU-R5F, DM-R5F, A53 | YES |
MCU | MCU-R5F, DM-R5F | YES | |
Wakeup | MCU-R5F, DM-R5F | YES | |
IPC | Main | MCU-R5F, DM-R5F, A53, C75 | YES |
MCAN | MCU | MCU-DM-R5F | YES |
MCASP | Main | DM-R5F, C75 | YES |
MCSPI | Main | MCU-R5F, DM-R5F | YES |
MCU | MCU-R5F, DM-R5F | YES | |
Pinmux | Main | MCU-R5F, DM-R5F | YES |
MCU | MCU-R5F, DM-R5F | YES | |
Wakeup | MCU-R5F, DM-R5F | YES | |
SOC | NA | MCU-R5F, DM-R5F, A53, C75 | YES |
SCIClient | NA | MCU-R5F, DM-R5F, A53, C75 | YES |
UART | Main | MCU-R5F, DM-R5F, A53, C75 | YES |
MCU | MCU-R5F, DM-R5F | YES | |
Wakeup | DM-R5F | YES | |
UDMA | Main | DM-R5F, A53 | YES |
Peripheral | Supported CPUs | SysConfig Support |
---|---|---|
Flash | DM-R5F | YES |
LED | MCU-R5F | YES |
SDL Module | Supported CPUs | SysConfig Support |
---|---|---|
MCRC | MCU-R5F | NO |
ESM | MCU-R5F | NO |
VTM | MCU-R5F | NO |
DCC | MCU-R5F | NO |
RTI | MCU-R5F | NO |
POK | MCU-R5F | NO |
STOG | MCU-R5F | NO |
MTOG | MCU-R5F | NO |
POK | MCU-R5F | NO |
ECC | MCU-R5F | NO |
PBIST | MCU-R5F | NO |
LBIST | MCU-R5F | NO |
ID | Head Line | Module | Applicable Releases |
---|---|---|---|
SITSW-2569 | SBL was not unlocking the main domain control MMRs, before starting Linux on A53. | SBL | 8.6.0 |
SITSW-2547 | JTAG Unlock of cores not working with bootloader certificate DBG_FULL_ENABLE. | SBL | 8.6.0 |
SITSW-2343 | Board configuration missing changes required for CSI-RX | Board Configuration | 8.6.0 |
SITSW-2336 | SBL is not able to boot DM firmware generated using the Firmware Builder | SBL | 8.6.0 |
SITSW-2306 | IPC RP message length on linux example is 96 bytes instead of 512 bytes | IPC | 8.6.0 |
SITSW-2186 | OSPI DMA is not working on the HS-SE devices | OSPI, SBL | 8.6.0 |
SITSW-2512 | R5F IPC example appimage generated using CCS is not working | DM | 8.6.0 |
SITSW-2397 | SBL not able to write OSPI PHY pattern when expected PHY pattern missing from PHY offset | SBL | 8.6.0 |
SITSW-2057 | SBL not closing the Timer/disabling the interrupts before switching to application on DM R5 | SBL | 8.6.0 |
SITSW-1962 | R5 MPU configuration is not reset for all regions before configuring | MPU | 8.6.0 |
SITSW-1766 | Utility elf2rprc not generating correct appimage if data sections have different load and run addresses | MPU | 8.6.0 |
SITSW-2513 | Inconsistency in Sysconfig version used by SDK makefiles & CCS | Makefiles | 8.6.0 |
PROC_SDL-5747 | STOG example fails when run continuously. Single step execution works. | SDL | 8.6.0 |
PROC_SDL-6229 | PBIST MAIN INSTANCE is not working for positive test vector. | SDL | 8.6.0 |
ID | Head Line | Module | Reported in release | Workaround |
---|---|---|---|---|
MCUSDK-208 | gmake with -j can sometimes lock up Windows command prompt | Build | 8.6.0 | Use bash for windows as part of git for windows or don't use -j option |
SITSW-2701 | Running MCU LBIST on SBL causes JTAG connection issues to MCU R5F | LBIST | 9.0.0 | None |
SITSW-2737 | DM trace log is not generated on the WKUP UART after the DM is booted. | DM | 9.0.0 | None |
PROC_SDL-6299 | ECC is not supported for some instances. These are SDL_PSRAMECC0_PSRAM256X32E_ECC_AGGR, SDL_WKUP_ECC_AGGR1_SAM62A_DM_MCU_ECC_AGGR , SDL_MCU_MSRAM_256K1_MSRAM32KX64E_ECC_AGGR,SDL_MCU_R5FSS0_PULSAR_ULS_CPU0_ECC_AGGR, SDL_CPSW0_CPSW_3GUSS_CORE_ECC_CPSW_ECC_AGGR, SDL_MCU_MSRAM_256K0_MSRAM32KX64E_ECC_AGGR, SDL_CSI_RX_IF0_CSI_RX_IF_ECC_AGGR, SDL_MCU_ECC_AGGR0_SAM62A_MCU_MCU_ECC_AGGR , SDL_SA3_SS0_SA3SS_AM62A_DMSS_ECCAGGR , SDL_VPAC0_SAM62A_VPAC_WRAP_IVPAC_TOP_0_PAC_BASE_KSDW_ECC_AGGR, SDL_VPAC0_SAM62A_VPAC_WRAP_IVPAC_TOP_0_VPAC_LDC0_KSDW_ECC_AGGR, SDL_VPAC0_SAM62A_VPAC_WRAP_IVPAC_TOP_0_VPAC_VISS0_KSDW_ECC_AGGR, SDL_MCU_ECC_AGGR1_SAM62A_MCU_PULSAR_UL_ECC_AGGR, SDL_C7X256V0_SAM62A_C7XV_WRAP_ECC_AGGR, SDL_USB1_USB2SS_16FFC_USB2SS_CORE_ECC_AGGR, SDL_USB0_USB2SS_16FFC_USB2SS_CORE_ECC_AGGR, SDL_COMPUTE_CLUSTER0_SAM62A_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE0, SDL_COMPUTE_CLUSTER0_SAM62A_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE1, SDL_COMPUTE_CLUSTER0_SAM62A_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE2, SDL_COMPUTE_CLUSTER0_SAM62A_A53_512KB_WRAP_A53_DUAL_WRAP_CBA_WRAP_A53_DUAL_WRAP_CBA_COREPAC_ECC_AGGR_CORE3, | SDL | 9.0.0 | None. Support will be added in future release. |
PROC_SDL-6431 | VIM diagnostics for register read back are not supported. | SDL | 9.0.0 | None. Support will be added in future release. |
S.No | Head Line | Module |
---|---|---|
1 | The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK | NA |
2 | DDR PHY mode not supported for OSPI NAND SBL | Bootloader |