AM62Ax MCU+ SDK  09.00.00
SDL ECC

Introduction

This example shows setup and usage of some ECC Aggregators for a few events in the Main domain. It shows the following:

  • Setup of an ESM application callback to receive Single Error Correction (SEC) and Double Error Detection (DED) events and setup of ECC Aggregators in general
  • Triggering of ECC events for a small number of RAM IDs, including Interconnect type and Wrapper type
  • Printing out error information within the ECC callback upon reception of ECC events

The following use cases are implemented in this example:

Use Cases

Use Case Description
UC-1 Single DED error on WKUP ESM for wrapper RAM ID type
UC-2 Single SEC error on Main ESM for wrapper RAM ID type
UC-3 Parity error injection on Main ESM for interconnect RAM ID type
UC-4 Single DED error on Main ESM for wrapper RAM ID type

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 nortos
Toolchain ti-arm-clang
Board am62ax-sk
Example folder examples/sdl/ecc/

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

ECC Example Application
ECC_Example_init: Init MAIN ESM complete
ECC_Example_init: Init WKUP ESM complete
ECC_init: AGGR0 ECC Init complete
ECC_init: PSRAM ECC Init complete
ECC_init: MCU MCAN1 ECC Init complete
ESM Safety Example tests: starting
MCU MCAN1 Double bit error inject Example test UC-1: starting
MCU MCAN1 Double bit error inject test: pError address 0x04E10000 test complete and the value is 0x00000301
Waiting for ESM Interrupt
UC-1: Got Low priority ESM Interrupt
AGGR0 Single bit error inject Example test UC-2: starting
AGGR0 Single bit error inject test: Subtype 0x00000004 test complete
Waiting for ESM Interrupt
UC-2: Got High priority ESM Interrupt
AGGR0 Memory Parity inject Example test UC-3: starting
AGGR0 Single bit error self test: Subtype 0x00000001 test complete
Waiting for ESM Interrupt
UC-3: Memory Parity Error Test Complete
PSRAM0 Double bit error inject Example test UC-4: starting
PSRAM0 Double bit error inject test: pError address 0x00900000 test complete and the value is 0x00000301
Waiting for ESM Interrupt
UC-4: Got Low priority ESM Interrupt
ECC Safety Example tests: success
ECC UC-1 and UC-2 Test
All Use_Cases have passed.