Introduction
This example demostrates the McASP configured for an audio playback mode of operation. A headset with mic needs to be connected to the auido jack on am62ax-sk. The audio from the microphone will be played back to both the headset (Left & Right).
- Mcasp is configured in I2S mode
- Data transfer is on both channels (Left and Right)
Supported Combinations
| Parameter | Value |
| CPU + OS | c75ss0-0 freertos |
| r5fss0-0 nortos |
| Toolchain | ti-c7000 |
| ti-arm-clang |
| Board | am62ax-sk |
| Example folder | examples/drivers/mcasp/mcasp_playback_codec_aic32 |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Connect audio devices as mentioned in the introduction
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
See Also
MCASP
Sample Output
Shown below is a sample output when the application is run,
[MCASP] Audio playback example started.
Enter your response on UART terminal
Stop the demo? (y/n) : y