Introduction
This example shows usage of RP Message APIs to exchange messages between RTOS/NORTOS CPUs as well as exchange message with QNX on Cortex-A CPU.
- One "main" CPU, sends multi-byte messages to other "remote" CPUs using the RP Message APIs
- The "remote" CPUs, then echo back the same message to the main CPUs
- Once all messages are echoed the main CPU exits. The remote CPUs remain waiting to receive new messages.
Supported Combinations
Parameter | Value |
CPU + OS | mcu-r5fss0-0 freertos |
r5fss0-0 freertos |
Toolchain | ti-arm-clang |
Board | am62ax-sk |
Example folder | examples/drivers/ipc/ipc_rpmsg_echo_qnx |
Steps to Run the Example
- Note
- This is a
system
or multi-core project, so refer to system project build instructions for CCS project or makefiles when building the example.
- When using CCS projects to build, import the system CCS project and build it using the CCS project menu (see Using SDK with CCS Projects). This will build all the dependant CPU projects as well
- When using makefiles to build, build the system makefile using make command (see Using SDK with Makefiles). This will build all the dependant CPU makefiles as well.
- To run this demo, QNX needs to run on the Cortex A-core. Refer to Processor SDK QNX user guide to load and run this example.
See Also
IPC RPMessage
Sample Output
There is no direct output from the RTOS/NORTOS CPUs on the UART or CCS console. The output is seen on the QNX console on Cortex-A CPU.