AM62Ax MCU+ SDK  09.00.00
MCU BIST Check Result

Introduction

This example reads the MCU LBIST and MCU PBIST results and verifies it. SBL OSPI example starts the MCU LBIST and MCU PBIST before loading the MCU core. Once the MCU core is booted the results of the MCU PBIST and MCU LBIST can be verified by this example.

Supported Combinations

Parameter Value
CPU + OS mcu-r5fss0-0 nortos
Toolchain ti-arm-clang
Board am62ax-sk
Example folder examples/drivers/safety/reset_isolation

Steps

Sample Output

Shown below is a sample output when the application is run,

All tests have passed!!