SOC | Supported CPUs | EVM | Host PC |
---|---|---|---|
AM62Ax | MCU R5F, R5F | SK-AM62A-LP EVM (referred to as am62ax-sk in code) | Windows 10 64b or Ubuntu 18.04 64b |
Tools | Supported CPUs | Version |
---|---|---|
Code Composer Studio | MCU-R5F | 12.2.0 |
SysConfig | MCU-R5F, R5F | 1.15.0, build 2826 |
TI ARM CLANG | MCU-R5F, R5F | 2.1.2.LTS |
FreeRTOS Kernel | MCU-R5F, R5F | 10.4.3 |
OS | Supported CPUs | SysConfig Support |
---|---|---|
FreeRTOS Kernel | MCU-R5F, R5F | NA |
FreeRTOS POSIX | MCU-R5F | NA |
NO RTOS | MCU-R5F, R5F | NA |
Module | Supported CPUs | SysConfig Support | OS support |
---|---|---|---|
Address Translate | MCU-R5F, R5F | YES | FreeRTOS, NORTOS |
Cache | MCU-R5F, R5F | YES | FreeRTOS, NORTOS |
Clock | MCU-R5F, R5F | YES | FreeRTOS, NORTOS |
CycleCounter | MCU-R5F, R5F | NA | FreeRTOS, NORTOS |
Debug | MCU-R5F, R5F | YES | FreeRTOS, NORTOS |
Heap | MCU-R5F, R5F | NA | FreeRTOS, NORTOS |
Hwi | MCU-R5F, R5F | YES | FreeRTOS, NORTOS |
MPU | MCU-R5F, R5F | YES | FreeRTOS, NORTOS |
Semaphore | MCU-R5F, R5F | NA | FreeRTOS, NORTOS |
Task | MCU-R5F, R5F | NA | FreeRTOS |
Timer | MCU-R5F, R5F | YES | FreeRTOS, NORTOS |
SBL Mode | Supported CPUs | SysConfig Support | PHY Support | DMA Support | OS support |
---|---|---|---|---|---|
OSPI NAND | R5F | YES | No | Yes | NORTOS |
EMMC | R5F | YES | NA | NA | NORTOS |
UART | R5F | YES | NA | No | NORTOS |
Peripheral | Domain | Supported CPUs | SysConfig Support |
---|---|---|---|
DDR | Main | R5F | YES |
GPIO | MCU | MCU-R5F, R5F | YES |
Main | MCU-R5F, R5F | YES | |
I2C | Main | MCU-R5F, R5F | YES |
MCU | MCU-R5F, R5F | YES | |
Wakeup | MCU-R5F, R5F | YES | |
IPC | Main | MCU-R5F, R5F | YES |
MCAN | MCU | MCU-R5F | YES |
MCSPI | Main | MCU-R5F, R5F | YES |
MCU | MCU-R5F, R5F | YES | |
Pinmux | Main | MCU-R5F, R5F | YES |
MCU | MCU-R5F, R5F | YES | |
Wakeup | MCU-R5F, R5F | YES | |
SOC | NA | MCU-R5F, R5F | YES |
SCIClient | NA | MCU-R5F, R5F | YES |
UART | Main | MCU-R5F, R5F | YES |
MCU | MCU-R5F, R5F | YES | |
Wakeup | R5F | YES |
Peripheral | Supported CPUs | SysConfig Support |
---|---|---|
Flash | R5F | YES |
LED | MCU-R5F | YES |
SDL Module | Supported CPUs | SysConfig Support |
---|---|---|
MCRC | MCU-R5F | NO |
ESM | MCU-R5F | NO |
VTM | MCU-R5F | NO |
NA
ID | Head Line | Module | Reported in release | Workaround |
---|---|---|---|---|
SITSW-2186 | SBL OSPI DMA is not working on the HS-SE devices | Bootloader | 8.6.0 | Disable DMA on the OSPI NAND SBL example when HS-SE device is used |
ID | Head Line | Module | Reported in release | Workaround |
---|---|---|---|---|
MCUSDK-208 | gmake with -j can sometimes lock up Windows command prompt | Build | 7.3.0 | Use bash for windows as part of git for windows or don't use -j option |
S.No | Head Line | Module |
---|---|---|
1 | The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK | NA |
2 | PHY mode not supported for OSPI NAND SBL | Bootloader |