AM275 FreeRTOS SDK  12.00.00
unibase_binding.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2023 Texas Instruments Incorporated
3  * Copyright (c) 2023 Excelfore Corporation (https://excelfore.com)
4  *
5  * All rights reserved not granted herein.
6  * Limited License.
7  *
8  * Texas Instruments Incorporated grants a world-wide, royalty-free,
9  * non-exclusive license under copyrights and patents it now or hereafter
10  * owns or controls to make, have made, use, import, offer to sell and sell ("Utilize")
11  * this software subject to the terms herein. With respect to the foregoing patent
12  * license, such license is granted solely to the extent that any such patent is necessary
13  * to Utilize the software alone. The patent license shall not apply to any combinations which
14  * include this software, other than combinations with devices manufactured by or for TI ("TI Devices").
15  * No hardware patent is licensed hereunder.
16  *
17  * Redistributions must preserve existing copyright notices and reproduce this license (including the
18  * above copyright notice and the disclaimer and (if applicable) source code license limitations below)
19  * in the documentation and/or other materials provided with the distribution
20  *
21  * Redistribution and use in binary form, without modification, are permitted provided that the following
22  * conditions are met:
23  *
24  * * No reverse engineering, decompilation, or disassembly of this software is permitted with respect to any
25  * software provided in binary form.
26  * * any redistribution and use are licensed by TI for use only with TI Devices.
27  * * Nothing shall obligate TI to provide you with source code for the software licensed and provided to you in object code.
28  *
29  * If software source code is provided to you, modification and redistribution of the source code are permitted
30  * provided that the following conditions are met:
31  *
32  * * any redistribution and use of the source code, including any resulting derivative works, are licensed by
33  * TI for use only with TI Devices.
34  * * any redistribution and use of any object code compiled from the source code and any resulting derivative
35  * works, are licensed by TI for use only with TI Devices.
36  *
37  * Neither the name of Texas Instruments Incorporated nor the names of its suppliers may be used to endorse or
38  * promote products derived from this software without specific prior written permission.
39  *
40  * DISCLAIMER.
41  *
42  * THIS SOFTWARE IS PROVIDED BY TI AND TI"S LICENSORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING,
43  * BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
44  * IN NO EVENT SHALL TI AND TI"S LICENSORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
45  * CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA,
46  * OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY,
47  * OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
48  * POSSIBILITY OF SUCH DAMAGE.
49 */
64 #ifndef UNIBASE_BINDING_H_
65 #define UNIBASE_BINDING_H_
66 
71 #define UBB_DEFAULT_DEBUG_LOG_MEMORY (64*1024)
72 
76 #define UBB_MEMOUT_ENDMARK "---###---"
77 
81 #define UBB_DEFAULT_LOG_INITSTR "4,ubase:45"
82 
86 #ifndef UBB_GETENV
87 #define UBB_GETENV getenv
88 #endif
89 
90 #ifdef __cplusplus
91 extern "C" {
92 #endif
93 
103 int ubb_memory_out_init(char *mem, int size);
104 
112 
118 
125 int ubb_memory_out_lastline(char **str, int *size);
126 
135 int ubb_memory_out_alldata(char **rstr, int *size);
136 
142 int ubb_memory_file_out(const char *fname);
143 
149 
150 typedef uint64_t(*get64ts_t)(void);
156 
163 
164 #ifdef __cplusplus
165 }
166 #endif
167 
168 #endif
169 
unibase_init_para_t
initialization parameters
Definition: unibase.h:151
ubb_memory_out_buffer
char * ubb_memory_out_buffer(void)
return the memory pointer of memory_out
size
uint16_t size
Definition: tisci_boardcfg.h:1
ubb_default_initpara
void ubb_default_initpara(unibase_init_para_t *init_para)
return the default initialization parameters supported in the binding layer
get64ts_t
uint64_t(* get64ts_t)(void)
Definition: unibase_binding.h:150
ubb_memory_out_lastline
int ubb_memory_out_lastline(char **str, int *size)
return the most recent output line in memory_out
ubb_memory_out_alldata
int ubb_memory_out_alldata(char **rstr, int *size)
return the all written line data in the buffer
str
char str[32]
Definition: tisci_core.h:1
ubb_memory_out_close
int ubb_memory_out_close(void)
de-initialize memory_out function
ubb_memory_out_init
int ubb_memory_out_init(char *mem, int size)
initialize the internal memory_out function
ubb_memory_file_out
int ubb_memory_file_out(const char *fname)
write the data in memory_out buffer into a file
ubb_set_gptp_gettime64
void ubb_set_gptp_gettime64(get64ts_t func)
set gptptime function for ub_gptp_gettime64
ubb_unibase_easyinit
void ubb_unibase_easyinit(void)
initialize unibase with 'ubb_default_initpara'