|
AM275 FreeRTOS SDK
12.00.00
|
|
Go to the documentation of this file.
54 #include <board/pmic/pmic_lld/pmic.h>
81 typedef struct PMIC_Config_s {
106 typedef struct PMIC_Params_s {
struct PMIC_Params_s PMIC_Params
Forward declaration of PMIC_Params.
Definition: pmic.h:71
uint8_t qaWdogpin2
Definition: pmic.h:94
void PMIC_critSecStartFn(void)
Initiates the start of a critical section for PMIC operations. This function attempts to acquire a se...
void PMIC_init(void)
This function initializes the PMIC module.
uint8_t qaWdogpin1Func
Definition: pmic.h:96
void PMIC_close(PMIC_Handle handle)
Close PMIC driver.
void PMIC_critSecStopFn(void)
Concludes a critical section for PMIC operations. This function releases the semaphore,...
Parameters passed during PMIC_open()
Definition: pmic.h:106
PMIC_Handle PMIC_getHandle(uint32_t instanceId)
Get handle to PMIC driver.
Pmic_CoreHandle_t * pmicCoreHandle
Definition: pmic.h:84
Pmic_CoreCfg_t * pmicConfigData
Definition: pmic.h:82
uint32_t qaWdogDrvinstance
Definition: pmic.h:110
uint8_t qaWdogpin1
Definition: pmic.h:92
uint32_t mainDrvinstance
Definition: pmic.h:107
void PMIC_deinit(void)
This function de-initializes the PMIC module.
PMIC_Handle PMIC_open(uint32_t instanceId, const PMIC_Params *params)
Open PMIC driver.
uint8_t trigWdogPinFunc
Definition: pmic.h:90
PMIC driver configuration, these are filled by SysCfg based on the device that is selected.
Definition: pmic.h:81
struct PMIC_Config_s PMIC_Config
Forward declaration of PMIC_Config.
Definition: pmic.h:68
uint8_t qaWdogpin2Func
Definition: pmic.h:98
uint8_t wdogMode
Definition: pmic.h:86
uint8_t trigWdogPin
Definition: pmic.h:88
void * PMIC_Handle
Handle to the PMIC driver returned by PMIC_open()
Definition: pmic.h:65