|
AM275 FreeRTOS SDK
12.00.00
|
|
Go to the documentation of this file.
68 #define DP83TG721_LED_NUM (2U)
77 typedef struct Dp83tg721_Cfg_s
uint32_t srcMacStatusFrameType
Definition: dp83tg721.h:81
uint8_t enableCodecClock
Definition: dp83tg721.h:85
bool isMDIMaster
Definition: dp83tg721.h:79
uint8_t enableMediaClock
Definition: dp83tg721.h:83
void Dp83tg721_initCfg(Dp83tg721_Cfg *cfg)
Initialize DP83TC811 PHY specific config params.
bool enablePTPstatusFrames
Definition: dp83tg721.h:80
DP83TG721 PHY configuration parameters.
Definition: dp83tg721.h:78
uint8_t clockSource
Definition: dp83tg721.h:82
uint32_t mediaClkDiv
Definition: dp83tg721.h:87
uint8_t mediaClockMode
Definition: dp83tg721.h:84
uint32_t codecClkDiv
Definition: dp83tg721.h:86